Solid Edge Framework Type Library
Environment Object
Members 
Description
The menus and accelerators to a Window object. Defines the set of commands that can be run while a window associated to an environment is active.
Object Model
Environment ObjectAccelerators CollectionApplication ObjectSelectSet CollectionAddIns CollectionApplication ObjectApplicationEvents ObjectApplicationV8DocumentOpenEvent ObjectApplicationWindowEvents ObjectCommand ObjectCustomization ObjectDocuments CollectionEnvironments CollectionFeatureLibraryEvents ObjectFileUIEvents ObjectMatTable ObjectInsight ObjectNewFileUIEvents ObjectApplication ObjectSEECEvents ObjectShortcutMenuEvents ObjectSolidEdgeInsightXT ObjectSolidEdgeTCE ObjectWindows CollectionCommandBars CollectionCommandCategories CollectionEnvironments Collection
Remarks
The environment describes the menus and accelerators to the window. Additionally, the environment defines the set of commands that can be executed while a window associated to an environment is active. An environment is associated with zero to many windows.
See Also

Environment Members

Send comments on this topic.