Solid Edge Framework Type Library
FillStyle Object
Members 
Description
Defines the fill characteristics of an enclosed object.
Remarks
Fill characteristics are set and retrieved through the properties for the FillStyle object. These properties include the pattern type used, the color, the scale, and so forth for the area fill.
See Also

FillStyle Members

Send comments on this topic.