Solid Edge Framework Type Library
HighlightSet Object
Members 
Description
Represents an occurrence of a Highlight set in Assembly, Draft, Part, or Sheet Metal documents.
Remarks
A highlight set allows you to highlight objects as needed–that is, methods are provided that enable you to set colors, draw, add objects to the set, and remove objects from the set. You create a HighlightSet object through the HighlightSets collection object.
See Also

HighlightSet Members

Send comments on this topic.