Solid Edge Framework Type Library
Reference Object
Members 
Description
Represents an object that references another object (a part or assembly, for example).
Remarks
It consists of an object and a matrix that specifies where in the assembly the referenced object is located. For example, a part in an assembly may be used many times. The data regarding the construction of the part exists only once in the file. All occurrences of the part are references to the original part with a matrix that specifies the location of the specific occurrence.
See Also

Reference Members

Send comments on this topic.