Solid Edge Framework Type Library
TextStyles Collection
Members 
Description
A collection of TextStyle objects.
Remarks
The Add method creates a new TextStyle object from a copy of one. To customize this object, set the TextStyle object's properties as needed to set the characteristics. When you add a text style through the automation interface, a text style is added, but not the corresponding text character style. You must explicitly create a new TextCharStyle with the same name as that of the new TextStyle.
See Also

TextStyles Members

Send comments on this topic.