Solid Edge Framework Type Library
UnitOfMeasure Object
Members 
Description
The UnitOfMeasure object allows you to set and return the unit type and precision for each category, depending on the index of the unit.
Remarks
If you are not sure what type or category the UnitOfMeasure object represents, you can use the Type property to return the type constant.
See Also

UnitOfMeasure Members

Send comments on this topic.