Solid Edge Framework Type Library
TransformViewToGLProjection Method
Specifies the x value of the View coordinate.
Specifies the y value of the View coordinate.
Specifies the z value of the View coordinate.
Returns the x value of the OpenGL projection coordinate.
Returns the y value of the OpenGL projection coordinate.
Returns the z value of the OpenGL projection coordinate.
Description
Converts View coordinates to OpenGL projection coordinates.
Syntax
Visual Basic
Public Sub TransformViewToGLProjection( _
   ByVal ViewX As Double, _
   ByVal ViewY As Double, _
   ByVal ViewZ As Double, _
   ByRef GLX As Double, _
   ByRef GLY As Double, _
   ByRef GLZ As Double _
) 
Parameters
ViewX
Specifies the x value of the View coordinate.
ViewY
Specifies the y value of the View coordinate.
ViewZ
Specifies the z value of the View coordinate.
GLX
Returns the x value of the OpenGL projection coordinate.
GLY
Returns the y value of the OpenGL projection coordinate.
GLZ
Returns the z value of the OpenGL projection coordinate.
See Also

View Object  | View Members

Send comments on this topic.