Solid Edge Framework Type Library
Window Object
Members 
Description
Provides support for adjusting the size of the actual viewing area.
Object Model
Window ObjectApplication ObjectSelectSet CollectionAddIns CollectionApplication ObjectApplicationEvents ObjectApplicationV8DocumentOpenEvent ObjectApplicationWindowEvents ObjectCommand ObjectCustomization ObjectDocuments CollectionEnvironments CollectionFeatureLibraryEvents ObjectFileUIEvents ObjectMatTable ObjectInsight ObjectNewFileUIEvents ObjectApplication ObjectSEECEvents ObjectShortcutMenuEvents ObjectSolidEdgeInsightXT ObjectSolidEdgeTCE ObjectWindows CollectionSelectSet CollectionView ObjectDisplayEvents ObjectGLDisplayEvents ObjectRenderEvents ObjectViewEvents ObjectWindow Object
Remarks
A window is either application- or document-centric. Application-centric windows reside in the Application>Windows collection. Document-centric windows reside in the Document>Windows collection and the Application>Windows collection. The Application>Windows collection can be thought of as the sum of all windows in each document plus all other windows.
See Also

Window Members

Send comments on this topic.