Solid Edge Framework Type Library
variable Object
Members 
Description
Associates a name with a numeric value.
Remarks
This numeric value can be a constant, or it can be derived through a formula. Data for the variable is set and/or returned through the Variable object's properties. A Variable object is created through the Add method of the Variables collection object. After the Variable, object is created, its name, value, and formula can be modified through individual properties.
See Also

variable Members

Send comments on this topic.