Angle | Sets and returns the angular rotation of the referenced object. |
Application | Returns the active application object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
DetailedStatus | Returns the detailed status of the Relation3d object. |
Index | Returns the numeric index for the active object. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
Occurrence1 | Returns the first Occurrence object for the referenced relationship object. |
Occurrence2 | Returns the second Occurrence object for the referenced relationship object. |
Parent | Returns the parent object for the referenced object. |
RangedAngle | |
RangeHigh | |
RangeLow | |
Status | Returns the status (a member of the Relation3dStatusConstants constant set) of the referenced Part. |
Suppress | Temporarily suppresses the referenced object. |
Type | A member of the ObjectType constant set. |