Solid Edge Assembly Type Library
GetElement2 Method
Specifies whether the returned object is a TopologyReference.
Description
Returns the second element in this relationship.
Syntax
Visual Basic
Public Function GetElement2( _
   ByRef IsTopologyReference As Boolean _
) As Object
Parameters
IsTopologyReference
Specifies whether the returned object is a TopologyReference.
Remarks
This method returns TopologyReference information for the second of two elements constrained by the relationship.
Example
Private Sub GetElement_Click(sender As Object, e As EventArgs) Handles GetElement1.Click
    Dim objApp As SolidEdgeFramework.Application = Nothing
    Dim objAsmDoc As SolidEdgeAssembly.AssemblyDocument = Nothing
    Dim objrels As SolidEdgeAssembly.Relations3d = Nothing
    Dim objrel As Object = Nothing

    Dim objele1 As Object = Nothing
    Dim objele2 As Object = Nothing

    Dim objele1TR As SolidEdgeAssembly.TopologyReference = Nothing
    Dim objele2TR As SolidEdgeAssembly.TopologyReference = Nothing
    Dim objele1R As SolidEdgeFramework.Reference = Nothing
    Dim objele2R As SolidEdgeFramework.Reference = Nothing

    Dim boolval1 As Boolean = Nothing
    Dim boolval2 As Boolean = Nothing

    Dim objocc1 As SolidEdgeAssembly.Occurrence = Nothing
    Dim objocc2 As SolidEdgeAssembly.Occurrence = Nothing

    Dim objTopOcc1 As Object = Nothing
    Dim aSubOccs1(0 To 4) As Object
    Dim numSubOcc1 As Integer
    Dim numBoundSubOcc1 As Integer

    Dim objTopOcc2 As Object = Nothing
    Dim aSubOccs2(0 To 4) As Object
    Dim numSubOcc2 As Integer
    Dim numBoundSubOcc2 As Integer

    Dim sName1 As String
    Dim sName2 As String

    Dim strRetStatusMsg As String

    Dim lCount As Integer
    Dim lIndex As Integer

    Try
        ' Create/get the application with specific settings
        objApp = GetObject(, "SolidEdge.Application")
        ' open the document mentioned in the doc files.
        objAsmDoc = objApp.ActiveDocument
        objrels = objAsmDoc.Relations3d
        lCount = objrels.Count
        For lIndex = 1 To lCount

            objrel = objrels.Item(lIndex)

            If objrel.Type <> SolidEdgeFramework.ObjectType.igAngularRelation3d Then

                objele1 = objrel.GetElement1(boolval1)
                objele2 = objrel.GetElement2(boolval2)

                objocc1 = objrel.Occurrence1
                objocc2 = objrel.Occurrence2

                sName1 = objocc1.Name
                sName2 = objocc2.Name

                If boolval1 Then
                    objele1TR = DirectCast(objele1, SolidEdgeAssembly.TopologyReference)
                    objele1TR.GetOccurrencesInPath(objTopOcc1, numSubOcc1, numBoundSubOcc1, aSubOccs1)

                Else
                    objele1R = DirectCast(objele1, SolidEdgeFramework.Reference)
                    objele1R.GetOccurrencesInPath(objTopOcc1, numSubOcc1, numBoundSubOcc1, aSubOccs1)

                End If

                If boolval2 Then
                    objele2TR = DirectCast(objele2, SolidEdgeAssembly.TopologyReference)
                    objele2TR.GetOccurrencesInPath(objTopOcc2, numSubOcc2, numBoundSubOcc2, aSubOccs2)
                Else
                    objele2R = DirectCast(objele2, SolidEdgeFramework.Reference)
                    objele2R.GetOccurrencesInPath(objTopOcc2, numSubOcc2, numBoundSubOcc2, aSubOccs2)
                End If

            End If

        Next lIndex
    Catch ex As Exception
        Clipboard.SetText(ex.ToString)
    End Try

End Sub
See Also

AngularRelation3d Object  | AngularRelation3d Members