Solid Edge Assembly Type Library
AssemblyCopy Object
Members 
Description
Object Model
AssemblyCopy ObjectApplication ObjectSelectSet CollectionAddIns CollectionApplication ObjectApplicationEvents ObjectApplicationV8DocumentOpenEvent ObjectApplicationWindowEvents ObjectCommand ObjectCustomization ObjectDocuments CollectionEnvironments CollectionFeatureLibraryEvents ObjectFileUIEvents ObjectMatTable ObjectInsight ObjectNewFileUIEvents ObjectApplication ObjectSEECEvents ObjectShortcutMenuEvents ObjectSolidEdgeInsightXT ObjectSolidEdgeTCE ObjectWindows Collection
Example
Imports System.IO
Imports System.Runtime.InteropServices

Module Example
    <STAThread()> _
    Sub Main()

        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim objAssemblyDocument As SolidEdgeAssembly.AssemblyDocument = Nothing
        Dim objAssemblyCopies As SolidEdgeAssembly.AssemblyCopies = Nothing
        Dim objAssemblyCopy As SolidEdgeAssembly.AssemblyCopy = Nothing
        Dim objCoordinateSystem As SolidEdgePart.CoordinateSystem
        Dim objSourceAssemblyDocument As SolidEdgeAssembly.AssemblyDocument
        Dim objSourceSolidEdgeDocument As SolidEdgeFramework.SolidEdgeDocument
        Dim objMirrorAsmRefPlane As SolidEdgeAssembly.AsmRefPlane = objAssemblyCopy.MirrorPlane

        Try
            OleMessageFilter.Register()

            objApplication = Marshal.GetActiveObject("SolidEdge.Application")
            objAssemblyDocument = objApplication.ActiveDocument
            objAssemblyCopies = objAssemblyDocument.AssemblyCopies
            objAssemblyCopy = objAssemblyCopies.Item("Assembly Copy_1")
            objCoordinateSystem = objAssemblyCopy.CoordinateSystem

            Console.Write("Add new components on update: ")
            Console.WriteLine(objAssemblyCopy.AddNewComponentsOnUpdate)
            Console.Write("IsFrozen: ")
            Console.WriteLine(objAssemblyCopy.IsFrozen)
            Console.Write("Is Out of Date: ")
            Console.WriteLine(objAssemblyCopy.IsOutOfDate)
            Console.Write("IncludeAssemblyFeatures: ")
            Console.WriteLine(objAssemblyCopy.IncludeAssemblyFeatures)

            Console.Write("Coordinate System: : ")
            Console.WriteLine(objCoordinateSystem.DisplayName)
            Console.Write("Source Document Name: ")
            Console.WriteLine(objAssemblyCopy.SourceFilename)

            Console.Write("Source Document Display Name: ")
            If Not (objAssemblyCopy.AssemblyCopyType = SolidEdgeAssembly.AssemblyCopyTypeConstants.seAssemblyCopyTypeMultiBodyPart) Then
                objSourceAssemblyDocument = objAssemblyCopy.SourceDocument
                Console.WriteLine(objSourceAssemblyDocument.DisplayName)
            Else
                objSourceSolidEdgeDocument = objAssemblyCopy.SourceDocument
                Console.WriteLine(objSourceSolidEdgeDocument.FullName)
            End If

            objMirrorAsmRefPlane = objAssemblyCopy.MirrorPlane

            If (objMirrorAsmRefPlane Is Nothing) Then
                Console.WriteLine("No mirror plane")
            Else
                Console.Write("Mirror plane: ")
                Console.WriteLine(objMirrorAsmRefPlane.Name)
            End If

            If (objAssemblyCopy.AssemblyCopyType = SolidEdgeAssembly.AssemblyCopyTypeConstants.seAssemblyCopyTypeDefault) Then
                Console.WriteLine("Copy Type: Default")
            ElseIf (objAssemblyCopy.AssemblyCopyType = SolidEdgeAssembly.AssemblyCopyTypeConstants.seAssemblyCopyTypeMirror) Then
                Console.WriteLine("Copy Type: Mirror")
            Else
                Console.WriteLine("Copy Type: MultiPart")
            End If

            If (objAssemblyCopy.Status = SolidEdgeAssembly.AssemblyCopyStatusConstants.seAssemblyCopyStatusOK) Then
                Console.WriteLine("Copy is OK")
            Else
                Console.WriteLine("Copy has a problem")
            End If
            Dim inArray As Array = Array.CreateInstance(GetType(System.Object), 2)
            Dim outArray As Array = Array.CreateInstance(GetType(SolidEdgeAssembly.Occurrence), 2)
            Dim fileArray As Array = Array.CreateInstance(GetType(System.Object), 2)
            Dim ActionArray As Array = Array.CreateInstance(GetType(SolidEdgeConstants.AssemblyCopyActionConstants), 2)
            Dim AdjustArray As Array = Array.CreateInstance(GetType(SolidEdgeConstants.AssemblyCopyPlaneConstants), 2)
            Dim EnumArray As Array = Array.CreateInstance(GetType(SolidEdgeConstants.AssemblyCopyUserConstants), 2)
            objAssemblyCopy.GetDefinition(inArray, outArray, ActionArray, AdjustArray, EnumArray)

            Dim x As Integer = 1
            For x = 0 To inArray.Length - 1 Step 1
                Dim occ As SolidEdgeAssembly.Occurrence = inArray(x)
                Console.Write(occ.Name)
                Console.Write("  input: ")
                If Not (outArray(x) Is Nothing) Then
                    occ = outArray(x)
                    Console.Write(occ.Name)
                Else
                    Console.Write(" Excluded")
                End If
                If (ActionArray(x) = SolidEdgeConstants.AssemblyCopyActionConstants.seAssemblyCopyActionInclude) Then
                    Console.Write("  Included  ")
                ElseIf (ActionArray(x) = SolidEdgeConstants.AssemblyCopyActionConstants.seAssemblyCopyActionMirror) Then
                    Console.Write("  Mirrored  ")
                ElseIf (ActionArray(x) = SolidEdgeConstants.AssemblyCopyActionConstants.seAssemblyCopyActionRotate) Then
                    Console.Write("  Rotated  ")
                ElseIf (ActionArray(x) = SolidEdgeConstants.AssemblyCopyActionConstants.seAssemblyCopyActionPending) Then
                    Console.Write("  Pending  ")
                Else
                    Console.Write("  Excluded  ")
                End If
                If (EnumArray(x) = SolidEdgeConstants.AssemblyCopyUserConstants.seAssemblyCopyDefault) Then
                    Console.Write("  Default  ")

                Else
                    Console.Write("  Modified  ")
                End If
                Console.WriteLine(AdjustArray(x))
            Next


        Catch ex As Exception
            Console.WriteLine(ex.Message)
        Finally
            OleMessageFilter.Revoke()
        End Try
    End Sub
End Module
See Also

AssemblyCopy Members  | Solid Edge ST5 - What's New