Private Sub Form_Load()
Dim objApp As SolidEdgeFramework.Application
Dim objDoc As SolidEdgeAssembly.AssemblyDocument
Dim objPart As SolidEdgeAssembly.Occurrence
Dim dblMatrix(1 To 16) As Double
Const TESTFILE = "T:\vbtests\testcases\cube.par"
' Report errors
Const PI = 3.14159265358979
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.AssemblyDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
' adding a part document to the assembly document
Set objPart = objDoc.Occurrences.AddByFilename(OccurrenceFileName:=TESTFILE)
' changing the location of the placed part using a matrix
dblMatrix(1) = 2
dblMatrix(2) = 0
dblMatrix(3) = 0
dblMatrix(4) = 0
dblMatrix(5) = 0
dblMatrix(6) = 2
dblMatrix(7) = 0
dblMatrix(8) = 0
dblMatrix(9) = 0
dblMatrix(10) = 0
dblMatrix(11) = 2
dblMatrix(12) = 0
dblMatrix(13) = 0.05
dblMatrix(14) = 0.05
dblMatrix(15) = 0.05
dblMatrix(16) = 1
Call objPart.PutMatrix(matrix:=dblMatrix, Replace:=True)
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objPart = Nothing
End Sub