Solid Edge Draft Type Library : Block Object |
Delete | Deletes the referenced object. |
Application | Returns the active application object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
DefaultView | Gets or sets the default view associated with a block. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
Name | Returns the name of the referenced object. |
OccurrenceCount | Returns the number of objects in the referenced collection. |
Parent | Returns the parent object for the referenced object. |
ScaleDimAndAnnot | Whether or not dimensions and annotations should use the block scale. |
Views | Block views collection |