Solid Edge Draft Type Library
BrokenOutSectionProfile Object
Members 
Description
Broken Out Section Profile
Object Model
BrokenOutSectionProfile ObjectApplication ObjectSelectSet CollectionAddIns CollectionApplication ObjectApplicationEvents ObjectApplicationV8DocumentOpenEvent ObjectApplicationWindowEvents ObjectCommand ObjectCustomization ObjectDocuments CollectionEnvironments CollectionFeatureLibraryEvents ObjectFileUIEvents ObjectMatTable ObjectInsight ObjectNewFileUIEvents ObjectApplication ObjectSEECEvents ObjectShortcutMenuEvents ObjectSolidEdgeInsightXT ObjectSolidEdgeTCE ObjectWindows CollectionDraftProfile ObjectApplication ObjectArcs2d CollectionBSplineCurves2d CollectionCircles2d CollectionDimensions CollectionEllipses2d CollectionEllipticalArcs2d CollectionLines2d CollectionRelations2d CollectionDrawingView ObjectApplication ObjectBrokenOutSectionProfiles CollectionCoordinateSystems2d CollectionDraftProfile ObjectCuttingPlanes CollectionDetailEnvelopes CollectionDVArcs2d CollectionDVBSplineCurves2d CollectionDVCircles2d CollectionDVEllipses2d CollectionDVEllipticalArcs2d CollectionDVLines2d CollectionDVLineStrings2d CollectionDVPoints2d CollectionModelMembers CollectionReference ObjectGraphicMembers CollectionHighlightDrawingViewMembers ObjectModelMembers CollectionDrawingView Object
Example
Imports System.IO
Imports System.Runtime.InteropServices

Public Class Form1

    Private Sub Button1_Click(sender As Object, e As EventArgs) Handles Button1.Click
        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim objFolder As DirectoryInfo
        Dim objFileInfo As FileInfo
        Dim objDocuments As SolidEdgeFramework.Documents = Nothing

        Dim objDraftDoc As SolidEdgeDraft.DraftDocument = Nothing
        Dim objSheet As SolidEdgeDraft.Sheet = Nothing
        Dim objDrawingViews As SolidEdgeDraft.DrawingViews = Nothing
        Dim objDrawingView As SolidEdgeDraft.DrawingView = Nothing

        Dim sectionView As SolidEdgeDraft.DrawingView
        Dim draftProfile As SolidEdgeDraft.DraftProfile
        Dim xmin, ymin, xmax, ymax As Double
        Dim xhalf, yhalf As Double
        Dim BOSProfile As SolidEdgeDraft.BrokenOutSectionProfile = Nothing
        Dim BOS As SolidEdgeDraft.BrokenOutSectionProfiles = Nothing
        Dim BOSProfiles As SolidEdgeDraft.BrokenOutSectionProfiles

        Try
            objApplication = Marshal.GetActiveObject("SolidEdge.Application")
            If objApplication Is Nothing Then
                ' Start Solid Edge
                objApplication = Activator.CreateInstance(Type.GetTypeFromProgID("SolidEdge.Application"))
                objApplication.Visible = True
            End If
            objFolder = GetTrainingFolder()
            objFileInfo = New FileInfo(Path.Combine(objFolder.FullName, "sbddaan.dft"))
            objDocuments = objApplication.Documents
            objDraftDoc = objDocuments.Open(objFileInfo.FullName)

            objSheet = objDraftDoc.ActiveSheet
            objDrawingViews = objSheet.DrawingViews
            objDrawingView = objDrawingViews.Item(1)

            BOSProfiles = objDrawingView.BrokenOutSectionProfiles
            BOSProfile = BOSProfiles.Add()

            draftProfile = BOSProfile.Profile
            draftProfile.BeginEdit()

            objDrawingView.Range(xmin, ymin, xmax, ymax)

            xhalf = xmin + (xmax - xmin) / 2
            yhalf = ymin + (ymax - ymin) / 2

            draftProfile.Circles2d.AddByCenterRadius(xhalf, yhalf, 0.25 * (xmax - xmin))

            draftProfile.EndEdit()

            sectionView = BOSProfile.TargetView
            BOSProfile.Depth = 0.2
            BOSProfile.DepthPlaneOffset = 0.1

            sectionView.Update()


        Catch ex As Exception
            MessageBox.Show(ex.ToString)
        End Try

    End Sub
    Function GetTrainingFolder() As DirectoryInfo
        Dim objInstallData As SEInstallDataLib.SEInstallData = Nothing
        Dim objInstallFolder As DirectoryInfo = Nothing
        Dim objTrainingFolder As DirectoryInfo = Nothing

        Try
            objInstallData = New SEInstallDataLib.SEInstallData
            objInstallFolder = New DirectoryInfo(objInstallData.GetInstalledPath())
            objTrainingFolder = New DirectoryInfo(Path.Combine(objInstallFolder.Parent.FullName, "Training"))
        Catch
        Finally
            If Not (objInstallData Is Nothing) Then
                Marshal.FinalReleaseComObject(objInstallData)
                objInstallData = Nothing
            End If
        End Try

        Return objTrainingFolder
    End Function



End Class
See Also

BrokenOutSectionProfile Members