Application | Returns the active application object. |
Area | Returns the area of the referenced object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
BendAngle | Returns the bend angle from the underlying sheet metal model. |
BendRadius | Returns the bend radius from the underlying sheet metal model. |
Document | Returns the document to which the referenced object belongs. |
DrawingView | Returns the DrawingView for this object. |
EdgeType | Returns the EdgeType for this object. |
Form | Returns the closure state of the referenced object. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
Key | Returns a key (a string) to find the object relative to its owning parents. |
KeyPointCount | Returns the number of keypoints/handles that are supported by the referenced object. |
Length | Specifies the length of the referenced object. |
ModelMember | Returns the ModelMember for this object. |
ModelWelds | Returns the ModelWelds collection object. |
Name | Returns the name of the referenced object. |
NodeCount | Returns the number of points on the referenced BSplineCurve2d object. |
Order | Returns the order of the curve for the referenced object. |
PoleCount | Returns the number of poles contained in the referenced BSplineCurve2d object. |
Reference | Returns a Reference object for this object. |
Relationships | Returns a collection of objects that are related to the referenced graphic object. |
Scope | Returns a constant that indicates the planarity, colinearity, or degeneracy for the referenced object. |
SegmentedStyleCount | Returns the number of segmented styles defined for the referenced graphic object. |
ShowHideEdgeOverride | Gets or sets a show/hide override on an edge or segment. |
Type | Specifies the type of the object being referenced. |