Solid Edge Draft Type Library
DraftFilePreferences Object Members
Overview
Collapse All
Expand All
Solid Edge Draft Type Library
: DraftFilePreferences Object
Public Properties
Application
Returns the active application object.
CenterOfMassBlockName
Gets or sets the block used for center of mass. Use empty string to clear this property.
CoordinateSystemBlockName
Gets or sets the block used for coordinate system. Use empty string to clear this property.
DVConfigChangesMakeViewsOutOfDate
DVCroppedEdgeProcessing
DVDeriveBendDirectionFromView
DVDeriveFillStyleFromPart
DVDeriveReferenceFromAssembly
DVDetailEnvelopeDisplayAsCircle
DVEdgeStyleName
Gets or sets the drawing view edge styles for the specified edge type.
DVEnableAlternatingHatchAngle
DVEnableAlternatingHatchSpacing
DVHatchRibsInSectionViews
DVIncludePMIAnnotations
DVIncludePMIDimensions
DVNailboardSetDisplayWhiteWiresAs
Specifies the color for displaying white wires in nailboard drawing views.
DVProjectionAngle
DVReferenceComponentsByConfigurations
Specifies whether show/hide settings are applied to reference components, e.g. ref planes, in drawing views using a configuration.
DVRetrieveDimensionsOnViewCreation
DVShowBoundaryEdges
DVShowCenterlines
DVShowDeformationFeatureOrigins
DVShowDeformationFeatureProfiles
DVShowDetailViewBorders
DVShowEdgesOfCuttingPlaneVertices
DVShowFillStyleInSectionViews
DVShowFillStyleInSectionWeldBeads
DVShowFlowlines
DVShowHiddenEdgesInConnectorViews
Specifies whether hidden edges in nailboard connector drawing views are shown by default.
DVShowHiddenEdgesInOrthographicViews
DVShowHiddenEdgesInPictorialViews
DVShowHiddenEdgesInSectionViews
DVShowHiddenOtherEdgesInOrthographicViews
DVShowHiddenOtherEdgesInPictorialViews
DVShowHiddenOtherTangentEdges
DVShowHiddenTangentEdges
DVShowTangentEdgesInOrthographicViews
DVShowTangentEdgesInPictorialViews
DVShowThreadsInSectionOnlyViews
DVShowTubeCenterlines
DVSolidFillSectionWeldBeads
DVStyleNameFromTable
Gets/Sets the drawing view style name for a given element type in the drawing view style mapping table.
DVThreadDisplayMode
GRIDAngle
Specifies the grid angle.
GRIDDisplayGridMode
Specifies whether grid is displayed as points or lines.
GRIDMajorLine
Specifies the grid major line spacing.
GRIDMinorSpaces
Specifies the number of minor spaces per major grid space.
GRIDSnapToGridMode
Specifies whether to snap to points or lines.
NumberSheetGroupsSeparately
Specifies whether sheet numbering is relative to all working sheets or to each sheet group.
Parent
Returns the parent object for the referenced object.
ViewerDataInclude2DModelSheet
ViewerDataIncludeBackgroundSheets
ViewerDataIncludeWorkingSheets
See Also
DraftFilePreferences Object
|
Solid Edge ST4 - What's New