Solid Edge Draft Type Library
Crop Property
Description
Specifies whether or not the contents of the referenced object are to be cropped.
Property type
Read-write property
Syntax
Visual Basic
Public Property Crop As Boolean
Remarks
Cropping extents are determined by the view frame based on the current values of the CropBottom, CropLeft, CropRight, and CropTop properties. If the Crop property is True, cropping occurs.
See Also

DrawingView Object  | DrawingView Members