Solid Edge Draft Type Library
EdgesUseModelColor Property
Description
Specifies whether or not edge and hatch style use model colors
Property type
Read-write property
Syntax
Visual Basic
Public Property EdgesUseModelColor As Boolean
Example
Imports System.IO
Imports System.Runtime.InteropServices

Module Example
    <STAThread()> _
    Sub Main()
        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim objDocuments As SolidEdgeFramework.Documents = Nothing
        Dim objDraftDocument As SolidEdgeDraft.DraftDocument = Nothing
        Dim objSections As SolidEdgeDraft.Sections = Nothing
        Dim objSection As SolidEdgeDraft.Section = Nothing
        Dim objSheet As SolidEdgeDraft.Sheet = Nothing
        Dim objDrawingViews As SolidEdgeDraft.DrawingViews = Nothing
        Dim objDrawingView As SolidEdgeDraft.DrawingView = Nothing

        Try
            OleMessageFilter.Register()

            ' Start Solid Edge
            objApplication = Activator.CreateInstance(Type.GetTypeFromProgID("SolidEdge.Application"))
            objApplication.Visible = True
            objDocuments = objApplication.Documents
            objDraftDocument = objDocuments.Open("anyfilename.dft")
            objSections = objDraftDocument.Sections
            objSection = objSections.WorkingSection

            ' Update all drawing views in all working sections.
            For Each objSheet In objSection.Sheets
                objDrawingViews = objSheet.DrawingViews
                For Each objDrawingView In objDrawingViews
                    objDrawingView.EdgesUseModelColor = True
                    objDrawingView.EdgesUsePartBaseColor = True
                    objDrawingView.EdgesUseAssemblyOverrideColor = False
                    objDrawingView.SectionHatchUseModelColor = True

                    objDrawingView.Update()
                Next
            Next
        Catch ex As Exception
            Console.WriteLine(ex.Message)
        Finally
            OleMessageFilter.Revoke()
        End Try
    End Sub
End Module
See Also

DrawingView Object  | DrawingView Members  | Solid Edge ST3 - What's New