Solid Edge Draft Type Library
EdgesUsePartBaseColor Property
Description
Specifies whether or not edge and hatch style use part base colors. 'EdgesUseModelColor' must be true before this option is honored.
Property type
Read-write property
Syntax
Visual Basic
Public Property EdgesUsePartBaseColor As Boolean
Example
Imports System.IO
Imports System.Runtime.InteropServices

Module Example
    <STAThread()> _
    Sub Main()
        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim objDocuments As SolidEdgeFramework.Documents = Nothing
        Dim objDraftDocument As SolidEdgeDraft.DraftDocument = Nothing
        Dim objSections As SolidEdgeDraft.Sections = Nothing
        Dim objSection As SolidEdgeDraft.Section = Nothing
        Dim objSheet As SolidEdgeDraft.Sheet = Nothing
        Dim objDrawingViews As SolidEdgeDraft.DrawingViews = Nothing
        Dim objDrawingView As SolidEdgeDraft.DrawingView = Nothing

        Try
            OleMessageFilter.Register()

            ' Start Solid Edge
            objApplication = Activator.CreateInstance(Type.GetTypeFromProgID("SolidEdge.Application"))
            objApplication.Visible = True
            objDocuments = objApplication.Documents
            objDraftDocument = objDocuments.Open("anyfilename.dft")
            objSections = objDraftDocument.Sections
            objSection = objSections.WorkingSection

            ' Update all drawing views in all working sections.
            For Each objSheet In objSection.Sheets
                objDrawingViews = objSheet.DrawingViews
                For Each objDrawingView In objDrawingViews
                    objDrawingView.EdgesUseModelColor = True
                    objDrawingView.EdgesUsePartBaseColor = True
                    objDrawingView.EdgesUseAssemblyOverrideColor = False
                    objDrawingView.SectionHatchUseModelColor = True

                    objDrawingView.Update()
                Next
            Next
        Catch ex As Exception
            Console.WriteLine(ex.Message)
        Finally
            OleMessageFilter.Revoke()
        End Try
    End Sub
End Module
See Also

DrawingView Object  | DrawingView Members  | Solid Edge ST3 - What's New