Solid Edge Draft Type Library
ModelMembers Property
Description
Returns the ModelMember collection of the Drawing View.
Property type
Read-only property
Syntax
Visual Basic
Public Property ModelMembers As ModelMembers
Example
Imports System.IO
Imports System.Runtime.InteropServices

Module Example
    <STAThread()> _
    Sub Main()
        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim objDraftDocument As SolidEdgeDraft.DraftDocument
        Dim objSheet As SolidEdgeDraft.Sheet = Nothing
        Dim objDrawingViews As SolidEdgeDraft.DrawingViews = Nothing
        Dim objDrawingView As SolidEdgeDraft.DrawingView = Nothing
        Dim objModelMembers As SolidEdgeDraft.ModelMembers = Nothing

        Try
            OleMessageFilter.Register()

            objApplication = Marshal.GetActiveObject("SolidEdge.Application")
            objDraftDocument = objApplication.ActiveDocument
            objSheet = objDraftDocument.ActiveSheet
            objDrawingViews = objSheet.DrawingViews
            objDrawingView = objDrawingView.Item(1)
            objModelMembers = objDrawingView.ModelMembers
            
        Catch ex As Exception
            Console.WriteLine(ex.Message)
        Finally
            OleMessageFilter.Revoke()
        End Try
    End Sub
End Module
See Also

DrawingView Object  | DrawingView Members