Solid Edge Draft Type Library
ModelLink Object
Members 
Description
Represents a member of the ModelLinks collection object.
Object Model
ModelLink ObjectApplication ObjectSelectSet CollectionAddIns CollectionApplication ObjectApplicationEvents ObjectApplicationV8DocumentOpenEvent ObjectApplicationWindowEvents ObjectCommand ObjectCustomization ObjectDocuments CollectionEnvironments CollectionFeatureLibraryEvents ObjectFileUIEvents ObjectMatTable ObjectInsight ObjectNewFileUIEvents ObjectApplication ObjectSEECEvents ObjectShortcutMenuEvents ObjectSolidEdgeInsightXT ObjectSolidEdgeTCE ObjectWindows CollectionModelNodes Collection
Remarks
The ModelLink object represents the relationship between a drawing view and a part, assembly, or weld. It differs from a ModelNode object in that the ModelLink is always at the root of the tree structure; ModelNodes are within the tree structure.
See Also

ModelLink Members