AlternatePositionMemberName | Returns the name of the alternate position assembly member that this ModelMember represents. |
Application | Returns the active application object. |
ComponentName | |
ComponentType | Returns the component type for the ModelMember. |
DeriveFillStyleFromPart | Specifies whether or not the fill style should be derived from the underlying part. |
DisplayAsReference | Displays the specified parts as reference parts. |
DisplayType | Specifies the display type for the ModelMember. |
DVArcs2d | Returns the DVArc2d collection of the ModelMember. |
DVBoundaries2d | Returns the drawing view hatch boundaries collection. |
DVBSplineCurves2d | Returns the DVBSplineCurve2d collection of the ModelMember. |
DVCircles2d | Returns the DVCircle2d collection of the ModelMember. |
DVEllipses2d | Returns the DVEllipse2d collection of the ModelMember. |
DVEllipticalArcs2d | Returns the DVEllipticalArc2d collection of the ModelMember. |
DVLines2d | Returns the DVLine2d collection of the ModelMember. |
DVLineStrings2d | Returns the DVLineString2d collection of the ModelMember. |
DVPoints2d | Returns the DVPoint2d collection of the ModelMember. |
FileName | Returns the file name for the referenced object. |
FillStyleName | Specifies the style used for the fill on sectioned parts. |
GraphicMembers | Returns the GraphicMember collection of the ModelMember. |
HatchAngle | Sets and returns the hatch angle that is applied to the selected parts. This value is always in radians. |
HatchSpacing | Sets and returns the hatch spacing that is applied to the selected parts. This value is always in millimeters. |
HiddenEdgeStyleName | Sets and returns the name of the hidden edge style that is applied to the referenced object. |
ImmediateParent | Returns the immediate parent for the referenced object. |
IsAlternatePosition | Specifies whether or not this ModelMember represents an alternate position of an alternate position assembly.. |
IsFlat | Returns True if the ModelMember represents a flat sheet metal part. |
IsPrimaryAlternatePosition | Specifies whether or not this ModelMember represents the primary position of an alternate position assembly. |
IsSimplified | Returns True if the ModelMember represents a simplified part. |
ModelMembers | Returns the ModelMember collection of the ModelMember. |
ModelNode | Returns the corresponding ModelNode object. |
Parent | Returns the parent object for the referenced object. |
ShowEdgesHiddenByOtherParts | Specifies whether edges hidden by other parts are to be displayed. |
ShowEdgesHiddenTangentEdgesHiddenByOtherParts | Specifies whether tangent edges that are hidden should be displayed. This setting can be set to TRUE only if ShowEdgesHiddenByOtherParts is set to TRUE. |
ShowEdgesHiddenTangentEdgesSelfHidden | Specifies whether tangent edges that are hidden should be displayed. This setting can be set to TRUE only if ShowHiddenEdges is set to TRUE. |
ShowFill | Specifies whether or not the fill will be shown on sectioned parts. |
ShowHiddenEdges | Specifies whether hidden edges are to be displayed. |
ShowSectionHatch | Specifies whether section hatches are to be displayed. |
ShowTangentEdges | Specifies whether tangent edges are to be displayed. |
TangentEdgeStyleName | Sets and returns the name of the tangent edge style that is applied to the referenced object. |
VisibleEdgeStyleName | Sets and returns the name of the visible edge style that is applied to the referenced object. |