Application | Returns the active application object. |
BottomNote1 | Sets and returns the Bottom Note 1 text for the referenced object. |
BottomNote2 | Sets and returns the Bottom Note 2 text for the referenced object. |
BottomNote3 | Sets and returns the Bottom Note 3 text for the referenced object. |
BottomNoteAngle | Returns the bottom note angle of the referenced ModelWeld object. |
BottomNoteCSize | Returns the bottom note compound size of the referenced ModelWeld object. |
BottomNoteDepth | Returns the bottom note depth of the referenced ModelWeld object. |
BottomNoteZ | Sets and returns the Bottom Note Z text for the referenced object. |
BottomPosOffset | Returns the bottom position offset of the referenced ModelWeld object. |
BottomTreatmentType | Sets and returns the treatment display style to use for the bottom treatment portion of the referenced object. |
BottomType | Sets and returns the bottom type for the referenced object. |
BottomTypeCompound | Returns the bottom weld compound symbol type of the referenced ModelWeld object. |
CenterType | Sets and returns the center type for the referenced object. |
CrossSectionArea | Returns the cross-sectional area of the referenced ModelWeld object. |
DashLine | Sets and returns the relative position of the dash lines for the referenced weld symbol object. |
Length | Specifies the length of the referenced object. |
OffsetTopBottom | Specifies whether the top and bottom weld types are offset or aligned. |
Parent | Returns the parent object for the referenced object. |
Symmetrical | Specifies whether or not the referenced object is symmetrical. |
Tail | Specifies whether the less than symbol appears at the end of the breaklline. |
TailNote | Sets and returns the tail note text. |
TailNote2 | Sets and returns the tail note text for the referenced ModelWeld object. |
TopNote1 | Sets and returns the Top Note 1 text. |
TopNote2 | Sets and returns the Top Note 2 text. |
TopNote3 | Sets and returns the Top Note 3 text. |
TopNoteAngle | Returns the top note angle of the referenced ModelWeld object. |
TopNoteCSize | Returns the top note compound size of the referenced ModelWeld object. |
TopNoteDepth | Returns the top note depth of the referenced ModelWeld object. |
TopNoteZ | Sets and returns the Top Note Z text. |
TopPosOffset | Returns the top position offset of the referenced ModelWeld object. |
TopTreatmentType | Sets and returns the display style to use for the top treatment portion of the referenced object. |
TopType | Sets and returns the top type for the referenced object. |
TopTypeCompound | Returns the top weld compound symbol type of the referenced ModelWeld object. |
WeldAllAround | Specifies whether or not the 'weld all around' display style is included in the referenced object. |
WeldBeadWeldImport | Specifies the weld import status of the referenced weld bead. |
WeldBeadWeldmentShape | Specifies the weldment shape of the referenced weld bead. |
WeldBeadWeldmentType | Specifies the weldment type of the referenced weld bead. |
WeldBeadWeldStandard | Specifies the weld standard of the referenced weld bead. |
WeldBeadWeldType | Specifies the weld type of the referenced weld bead. |
WeldInField | Specifies whether or not the 'weld in field' display style is included in the referenced object. |
ZSymbol | Specifies whether or not the Z weld symbol modifier is included in the referenced object. |