Public Methods
AddMember | This method adds a member object to the bolt hole circle. |
BringForward | Changes the display order of the referenced object by moving it in front of the first object that obscures it. |
BringToFront | Changes the display order of the referenced object by moving it in front of all other overlapping objects. |
Circle2d | This method returns the x and y coordinates of the center point of the referenced BoltHoleCircle object, as well as its radius. |
Copy | Places a copy of the referenced object on the clipboard. |
Cut | Moves the referenced object to the system clipboard. |
Delete | Deletes the referenced object. |
GetConnectElements3Objects | This method returns the 3 objects that define a bolt hole circle defined by 3 points. |
GetConnectElementsCenterRadius | This method returns the center object and the radius object that define the referenced BoltHoleCircle object. |
GetKeyPoint | Returns information about a specified key point. |
GetTrimArcEndPoints | Returns the start and end points of arc which is trimmed out of BHC. |
Item | The items in a collection. |
Range | Returns the high and low range values for the referenced object. |
RemoveMember | This method removes a specified member from the referenced object. |
Select | Selects the referenced object in the active window. |
SendBackward | Changes the display order of visible objects by moving the referenced object so that it is in back of the first object behind it. |
SendToBack | Changes the display order of visible objects by moving the referenced object behind all overlapping objects. |
SetTrimArcEndPoints | Sets the start and end points of arc which will be trimmed out of BHC. If both the points are same then BHC will be untrimmed to make it a full circle. |
Public Properties
Application | Returns the active application object. |
Count | Returns the number of objects in the referenced collection. |
Document | Returns the document to which the referenced object belongs. |
Index | Returns the numeric index for the active object. |
IsAcceptableConnectElementOrMember | This read-only Boolean property returns True if the object specified is on the same sheet as the referenced BoltHoleCircle object. |
IsDefinedBy2Points | Specifies whether BHC is defined by two points |
IsDefinedBy3Points | This read-only Boolean property returns True if the referenced BoltHoleCircle object is defined by 3 points. |
IsMember | This read-only Boolean property returns True if the object specified is a member of the referenced BoltHoleCircle object. |
Key | Returns a key (a string) to find the object relative to its owning parents. |
KeyPointCount | Returns the number of keypoints/handles that are supported by the referenced object. |
Layer | Sets and returns the named layer on which the referenced object resides. |
Name | Returns the name of the referenced object. |
Parent | Returns the parent object for the referenced object. |
Style | For collection objects, Body objects, RefPlane objects, Sketch objects, CoordinateSystem objects, CommandBarButton objects, SmartFrame2d objects, View objects, and TextCharStyle objects, Style is read-write. For all other objects, Style is read-only. |
TextScale | Sets and returns the text scale of the object. |
Type | Specifies the type of the object being referenced. |
ZOrder | Specifies the front-to-back order in which an object is displayed relative to other objects. |
See Also