Solid Edge FrameworkSupport Type Library
GetTrimArcEndPoints Method
Description
Returns the start and end points of arc which is trimmed out of BHC.
Syntax
Visual Basic
Public Sub GetTrimArcEndPoints( _
   ByRef x1 As Double, _
   ByRef y1 As Double, _
   ByRef z1 As Double, _
   ByRef x2 As Double, _
   ByRef y2 As Double, _
   ByRef z2 As Double _
) 
Parameters
x1
y1
z1
x2
y2
z2
Example
Imports System.Runtime.InteropServices
Public Class BoltHoleCircle

    Private Sub Button1_Click(sender As System.Object, e As System.EventArgs) Handles Button1.Click
        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim ObjDraftDoc As SolidEdgeDraft.DraftDocument = Nothing
        Dim objSheet As SolidEdgeDraft.Sheet = Nothing
        Dim objCircle As SolidEdgeFrameworkSupport.Circle2d = Nothing
        Dim objCircle2 As SolidEdgeFrameworkSupport.Circle2d = Nothing
        Dim objBoltHoleCircles As SolidEdgeFrameworkSupport.BoltHoleCircles = Nothing
        Dim objBoltHoleCircle As SolidEdgeFrameworkSupport.BoltHoleCircle = Nothing
        Dim objType As Type = Nothing
        Dim x1, y1, x2, y2 As Double
        Dim a1, b1, a2, b2 As Double

        Try
            ' Create/get the application with specific settings
            objApplication = Marshal.GetActiveObject("SolidEdge.Application")

            If objApplication Is Nothing Then
                ' Get the type from the Solid Edge ProgID
                objType = Type.GetTypeFromProgID("SolidEdge.Application")
                ' Start Solid Edge
                objApplication = Activator.CreateInstance(objType)
                ' Make Solid Edge visible
                objApplication.Visible = True
            End If
            'Get reference to active document
            ObjDraftDoc = objApplication.ActiveDocument

            'getting the Active Sheet object
            objSheet = ObjDraftDoc.ActiveSheet
            objBoltHoleCircles = objSheet.BoltHoleCircles

            objCircle = objSheet.Circles2d.AddByCenterRadius(x:=0.25, y:=0.25, Radius:=0.05)
            objCircle2 = objSheet.Circles2d.AddByCenterRadius(x:=0.5, y:=0.5, Radius:=0.05)

            objBoltHoleCircle = objBoltHoleCircles.AddBoltHoleCircleBy2Points( _
                                  objCircle, 0, _
                                  objCircle2, 0)
            If objBoltHoleCircle.IsDefinedBy2Points() = False Then
                MsgBox("Method IsDefinedBy2Points() failed.")
            End If

            objCircle.GetCenterPoint(x1, y1)
            objCircle2.GetCenterPoint(x2, y2)

            objBoltHoleCircle.SetTrimArcEndPoints(x1, y1, 0, x2, y2, 0)
            objBoltHoleCircle.GetTrimArcEndPoints(a1, b1, 0, a2, b2, 0)

        Catch ex As Exception
            MsgBox(ex.ToString)
        End Try

    End Sub
End Class
See Also

BoltHoleCircle Collection  | BoltHoleCircle Members