Private Sub Form_Load()
Dim objApp As SolidEdgeFrameWork.Application
Dim objDoc As SolidEdgeDraft.DraftDocument
Dim objSheet As SolidEdgeDraft.Sheet
Dim objCenterLines As SolidEdgeFrameworkSupport.CenterLines
Dim objCenterLine As SolidEdgeFrameworkSupport.CenterLine
Dim objAttributeSet As Object
Dim bAttribPresent As Boolean
' Report errors
Const PI = 3.14159265358979
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
'getting the Active Sheet object
Set objSheet = objDoc.ActiveSheet
' Get the CenterLines object on the active sheet
Set objCenterLines = objSheet.CenterLines
' Draw a CenterLine on the active sheet
Set objCenterLine = objCenterLines.Add(x1:=0.25, y1:=0.15, z1:=0, _
x2:=0.25, y2:=0.35, z2:=0)
'Create an AttributeSet with Add method
Set objAttributeSet = objCenterLine.AttributeSets.Add("MyAttrib Set")
'Get the boolean value of IsAttributeSetPresent
bAttribPresent = objCenterLine.IsAttributeSetPresent(Name:="MyAttrib Set")
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objSheet = Nothing
Set objAttributeSet = Nothing
Set objCenterLines = Nothing
Set objCenterLine = Nothing
End Sub