BringForward | Changes the display order of the referenced object by moving it in front of the first object that obscures it. |
BringToFront | Changes the display order of the referenced object by moving it in front of all other overlapping objects. |
ConnectObjects | This method connects the two specified objects at their respective center lines. |
Copy | Places a copy of the referenced object on the clipboard. |
Cut | Moves the referenced object to the system clipboard. |
Delete | Deletes the referenced object. |
GetCenter | Returns the object and a point on that object at which the Referenced Arc CenterLine object have center. |
GetCenterPoint | Returns the point that is the center of the referenced object. |
GetEnd | Returns the object and a point on that object at which the Referenced CenterLine object terminates. |
GetEndPoint | Returns the coordinates of the end point of the referenced object. |
GetKeyPoint | Returns information about a specified key point. |
GetStart | Returns the object and a point on that object at which the Referenced CenterLine object starts. |
GetStartPoint | Returns the coordinates of the start point for the referenced object. |
Move | Moves the referenced object. |
Range | Returns the high and low range values for the referenced object. |
Rotate | Rotates the referenced object about the point specified by the angle in radians. |
Scale | Scales the referenced object by a specified factor. |
Select | Selects the referenced object in the active window. |
SendBackward | Changes the display order of visible objects by moving the referenced object so that it is in back of the first object behind it. |
SendToBack | Changes the display order of visible objects by moving the referenced object behind all overlapping objects. |
SetCenter | Relocates the center of the referenced Arc CenterLine object. |
SetCenterPoint | Relocates the center point of the specified object. |
SetEnd | Relocates the end of the referenced CenterLine object. |
SetEndPoint | Sets the x and y values of the end point for the referenced object. |
SetKeyPoint | Sets the position for a specified key point. |
SetStart | Relocates the start of the referenced CenterLine object. |
SetStartPoint | Relocates the starting point of the referenced object. |