Imports System.Runtime.InteropServices
Public Class ChangeCenterPoint
Private Sub btnChangeCenterPoint_Click(sender As System.Object, e As System.EventArgs) Handles btnChangeCenterPoint.Click
Dim objApplication As SolidEdgeFramework.Application = Nothing
Dim objDraftDoc As SolidEdgeDraft.DraftDocument = Nothing
Dim objSheet As SolidEdgeDraft.Sheet = Nothing
Dim objCenterLines As SolidEdgeFrameworkSupport.CenterLines = Nothing
Dim objCenterLine As SolidEdgeFrameworkSupport.CenterLine = Nothing
Dim objType As Type = Nothing
Try
' Create/get the application with specific settings
objApplication = Marshal.GetActiveObject("SolidEdge.Application")
If objApplication Is Nothing Then
' Get the type from the Solid Edge ProgID
objType = Type.GetTypeFromProgID("SolidEdge.Application")
' Start Solid Edge
objApplication = Activator.CreateInstance(objType)
' Make Solid Edge visible
objApplication.Visible = True
End If
objDraftDoc = objApplication.ActiveDocument
'getting the Active Sheet object
objSheet = objDraftDoc.ActiveSheet
' Get the CenterLines object on the active sheet
objCenterLines = objSheet.CenterLines
' Draw a Center arc on the active sheet
objCenterLine = objCenterLines.AddCenterArc(Nothing, 0.05, 0.02, 0.0#, False, Nothing, 0.1, 0.04, 0.0#, False, Nothing, 0.2, 0.03, 0.0#, False, False)
' Set the Center Point
Call objCenterLine.SetCenterPoint(x:=0.15, y:=0.03, z:=0)
Catch ex As Exception
MsgBox(ex.ToString)
End Try
End Sub
End Class