Private Sub Form_Load()
Dim objApp As SolidEdgeFrameWork.Application
Dim objDoc As SolidEdgeDraft.DraftDocument
Dim objSheet As SolidEdgeDraft.Sheet
Dim objCenterLines As SolidEdgeFrameworkSupport.CenterLines
Dim objCenterLine As SolidEdgeFrameworkSupport.CenterLine
Dim dblX As Double, dblY As Double, dblZ As Double
Dim cHndType As HandleType
Dim cKPType As KeyPointType
' Report errors
Const PI = 3.14159265358979
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
'getting the Active Sheet object
Set objSheet = objDoc.ActiveSheet
' Get the CenterLines object on the active sheet
Set objCenterLines = objSheet.CenterLines
' Draw a CenterLine on the active sheet
Set objCenterLine = objCenterLines.Add(x1:=0.25, y1:=0.15, z1:=0, _
x2:=0.25, y2:=0.35, z2:=0)
' Set a KeyPoint
Call objCenterLine.SetKeyPoint(Index:=1, x:=0.25, y:=0.2, z:=0)
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objSheet = Nothing
Set objCenterLines = Nothing
Set objCenterLine = Nothing
End Sub