Specifies the graphic object at which the centerline starts.
Specifies the coordinates of the locate point for the StartObject. This point is used as a proximity point while calculating the key point.
Specifies the coordinates of the locate point for the StartObject. This point is used as a proximity point while calculating the key point.
Specifies the coordinates of the locate point for the StartObject. This point is used as a proximity point while calculating the key point.
Specifies whether the StartObject or a key point of that object is to be used for measuring. If True, the element is selected for the dimension's start point; if False, the nearest key point is selected.
Description
Relocates the start of the referenced CenterLine object.
Syntax
Visual Basic
Public Sub SetStart( _
ByVal StartObj As Object, _
ByVal x As Double, _
ByVal y As Double, _
ByVal z As Double, _
ByVal keyPoint As Boolean _
)
Parameters
StartObj
Specifies the graphic object at which the centerline starts.
x
Specifies the coordinates of the locate point for the StartObject. This point is used as a proximity point while calculating the key point.
y
Specifies the coordinates of the locate point for the StartObject. This point is used as a proximity point while calculating the key point.
z
Specifies the coordinates of the locate point for the StartObject. This point is used as a proximity point while calculating the key point.
keyPoint
Specifies whether the StartObject or a key point of that object is to be used for measuring. If True, the element is selected for the dimension's start point; if False, the nearest key point is selected.
Remarks
The start of the centerline can reference a new object or another point on the same object. It can also be placed with respect to the object or to a key point on that object. If the CenterLine object is placed with respect to a key point, the point of reference is the key point.