Private Sub Form_Load()
Dim objApp As SolidEdgeFrameWork.Application
Dim objDoc As SolidEdgeDraft.DraftDocument
Dim objSheet As SolidEdgeDraft.Sheet
Dim objDatumPoints As SolidEdgeFrameworkSupport.DatumPoints
Dim objdatumpoint1 As SolidEdgeFrameworkSupport.DatumPoint
Dim objdatumpoint2 As SolidEdgeFrameworkSupport.DatumPoint
Dim objdatumpoint3 As SolidEdgeFrameworkSupport.DatumPoint
Dim lngZorder1 As Long
Dim lngZorder2 As Long
Dim lngZorder3 As Long
Dim lngZorder4 As Long
' Report errors
Const PI = 3.14159265358979
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
'Get the Active Sheet object
Set objSheet = objDoc.ActiveSheet
'create a collection of datumpoints
Set objDatumPoints = objSheet.DatumPoints
'add datumpoints
Set objdatumpoint1 = objDatumPoints.Add(x1:=0.2, y1:=0.2, z1:=0)
Set objdatumpoint2 = objDatumPoints.Add(x1:=0.2, y1:=0.2, z1:=0)
Set objdatumpoint3 = objDatumPoints.Add(x1:=0.2, y1:=0.2, z1:=0)
'get zorder of first datumpoint
lngZorder1 = objdatumpoint1.ZOrder
'bring to front
Call objdatumpoint1.BringToFront
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objSheet = Nothing
Set objDatumPoints = Nothing
Set objdatumpoint1 = Nothing
Set objdatumpoint2 = Nothing
Set objdatumpoint3 = Nothing
End Sub