Solid Edge FrameworkSupport Type Library : DatumPoint Object |
BringForward | Changes the display order of the referenced object by moving it in front of the first object that obscures it. |
BringToFront | Changes the display order of the referenced object by moving it in front of all other overlapping objects. |
Copy | Places a copy of the referenced object on the clipboard. |
Cut | Moves the referenced object to the system clipboard. |
Delete | Deletes the referenced object. |
Duplicate | Copies the referenced object to a specified location, creating a new instance of the object with the same property values as the original. |
GetCenter | Returns the element for the referenced DatumPoint object. |
GetDisplayData | |
GetElement | Returns the element for the referenced DatumPoint object. |
GetFreeSpacePoint | Returns the coordinates of the terminal connect point for a leader line that belongs to the active dimensioning object. |
GetKeyPoint | Returns information about a specified key point. |
GetRectangularDatumPointWidthAndHeight | Sets and returns rectangular datum point's width and height. |
Move | Moves the referenced object. |
PromoteToCurrentVersion | Promotes datum point to the latest version behavior, the same as if placing a new object. |
Range | Returns the high and low range values for the referenced object. |
Select | Selects the referenced object in the active window. |
SendBackward | Changes the display order of visible objects by moving the referenced object so that it is in back of the first object behind it. |
SendToBack | Changes the display order of visible objects by moving the referenced object behind all overlapping objects. |
SetCenter | Specifies a new location for a CenterMark or DatumPoint object. |
SetElement | Sets the element for the referenced DatumPoint object. |
SetFreeSpacePoint | Specifies the coordinates of the terminal connect point for a leader line belonging to the referenced dimensioning object. |
SetKeyPoint | Sets the position for a specified key point. |
SetRectangularDatumPointWidthAndHeight | Sets and returns rectangular datum point's width and height. |
Application | Returns the active application object. |
AreaSize | Sets and returns the area size for the referenced DatumPoint object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
Document | Returns the document to which the referenced object belongs. |
HidePMI | Show or Hide the referenced PMI Datum Point object. |
Index | Returns the numeric index for the active object. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
Key | Returns a key (a string) to find the object relative to its owning parents. |
KeyPointCount | Returns the number of keypoints/handles that are supported by the referenced object. |
Layer | Sets and returns the named layer on which the referenced object resides. |
Name | Returns the name of the referenced object. |
Parent | Returns the parent object for the referenced object. |
Plane | For dimensions, returns the planar object used by the dimension to measure an object. For profiles, CopiedPart objects, and CopyConstruction objects, sets and returns the associated RefPlane object. |
PMIName | Get and set the name of reference PMI annotation object. |
PMIPlane | |
PMITrackDistance | |
PointType | Sets and returns the point type for the referenced DatumPoint object. |
Style | For collection objects, Body objects, RefPlane objects, Sketch objects, CoordinateSystem objects, CommandBarButton objects, SmartFrame2d objects, View objects, and TextCharStyle objects, Style is read-write. For all other objects, Style is read-only. |
TextScale | Sets and returns the text scale of the object. |
Type | Specifies the type of the object being referenced. |
ZOrder | Specifies the front-to-back order in which an object is displayed relative to other objects. |