Private Sub Form_Load()
Dim objApp As SolidEdgeFrameWork.Application
Dim objDoc As SolidEdgeDraft.DraftDocument
Dim objSheet As SolidEdgeDraft.Sheet
Dim objDatumPoints As SolidEdgeFrameworkSupport.DatumPoints
Dim objDatumPoint As SolidEdgeFrameworkSupport.DatumPoint
Dim dblXmin As Double, dblYmin As Double
Dim dblXmax As Double, dblYmax As Double
' Report errors
Const PI = 3.14159265358979
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
'Get the Active Sheet object
Set objSheet = objDoc.ActiveSheet
'create a datumpoints' collection.
Set objDatumPoints = objSheet.DatumPoints
'add a datumpoint to collection
Set objDatumPoint = objDatumPoints.Add(x1:=0.2, y1:=0.2, z1:=0)
Call objDatumPoint.Range(XMinimum:=dblXmin, YMinimum:=dblYmin, _
XMaximum:=dblXmax, YMaximum:=dblYmax)
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objSheet = Nothing
Set objDatumPoints = Nothing
Set objDatumPoint = Nothing
End Sub