Solid Edge FrameworkSupport Type Library
DualModeVerticalGap Property
Collapse All
Expand All
Solid Edge FrameworkSupport Type Library
>
DimensionStyle Object
: DualModeVerticalGap Property
Description
Sets and returns the vertical gap distance between Dimension Value text when the DualModeDisplay property is True.
Property type
Read-write property
Syntax
Visual Basic
Public Property DualModeVerticalGap As Double
Remarks
The value is expressed as a ratio of dimension text height.
See Also
DimensionStyle Object
|
DimensionStyle Members