Private Sub Form_Load()
Dim objApp As SolidEdgeFrameWork.Application
Dim objDoc As SolidEdgeDraft.DraftDocument
Dim objSheet As SolidEdgeDraft.Sheet
Dim objArc As SolidEdgeFrameworkSupport.Arc2d
Dim objDimension As SolidEdgeFrameworkSupport.Dimension
Dim bConstraint As Boolean
' Report errors
Const PI = 3.14159265358979
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
'getting the Active Sheet object
Set objSheet = objDoc.ActiveSheet
'create an arc2d
Set objArc = objSheet.Arcs2d.AddByCenterStartEnd(xCenter:=0.2, _
yCenter:=0.2, xStart:=0.1, yStart:=0.1, xEnd:=0.3, yEnd:=0.3)
'create a dimension
Set objDimension = objSheet.Dimensions.AddLength(Object:=objArc)
'get constraint
bConstraint = objDimension.Constraint
'set constraint to true
objDimension.Constraint = True
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objSheet = Nothing
Set objDimension = Nothing
Set objArc = Nothing
End Sub