AbsoluteTrackDistance | |
AngleClockwise | Returns True if the referenced Dimension object measures the angle clockwise. |
AngleCompliment | Specifies whether or not the referenced dimension measures the compliment value. |
Application | Returns the active application object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
Axis | Sets and returns the object used as the axis for the referenced object. It must be a line. |
BreakDistance | Sets and returns the break distance for the referenced Dimension object. |
BreakPosition | Sets and returns the break position for the referenced Dimension object. |
ChamferDimensionMode | Returns the mode of chamfer dimension (along axis, callout perpendicular, or callout parallel). |
Constraint | Sets and returns the Constraint property for the referenced dimension object. |
DimensionType | Sets and returns the type of dimension for the referenced object. |
DisplayHalf | Sets and returns the Display Half flag for symmetrical and radial diameter dimensions. |
DisplayName | This read-only String property returns the display name for the referenced object. |
DisplayType | Sets and returns the display type for the referenced object. |
Document | Returns the document to which the referenced object belongs. |
Expose | |
ExposeName | This read-write String property sets and returns the name of the referenced object when the object is exposed as a custom property. |
Formula | Sets and returns the formula of the referenced Variable object. |
GroupMemberType | Returns the type of group(Stack, Chain, Coordinate or Not a Group) to which referenced dimension object belongs. |
HidePMI | Show or Hide the referenced PMI Dimension object. |
HoleClassString | Hole Class String. This string must match a class in the standards table, e.g. H7. |
Index | Returns the numeric index for the active object. |
InhibitZeroToleranceDisplay | Inhibit display of zero tolerance value |
Inspection | Determines whether or not an inspection bubble is applied to the referenced Dimension object. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
Jogged | Specifies whether or not the referenced Dimension object is jogged. |
Key | Returns a key (a string) to find the object relative to its owning parents. |
KeyPointCount | Returns the number of keypoints/handles that are supported by the referenced object. |
Layer | Sets and returns the named layer on which the referenced object resides. |
Leader | Specifies whether or not the referenced object has a leader line. |
LeaderDistance | Sets and returns the leader distance of the referenced Dimension object. |
MeasureLineDirection | Determines the direction of measurement for coordinate dimensions. |
MeasurementAxisDirection | Specifies the direction in which the linear distance is measured for the referenced Dimension object. |
MeasurementAxisEx | Sets and returns the axis mode of a Dimension. |
Name | Returns the name of the referenced object. |
OffsetLeader | Specifies whether or not the referenced Dimension object has the offset leader line. |
OriginLineDirection | Specifies the orientation of the origin line for coordinate dimensions. |
OverrideChamferAngleString | Returns the chamfer dimension angle override string. |
OverrideString | Sets and returns the override value set on the referenced Dimension object. |
Parent | Returns the parent object for the referenced object. |
PMIPlane | |
PMITrackDistance | |
PrefixDisplayedText | Returns the evaluated Prefix text. |
PrefixInside | Specifies whether or not prefix text for the referenced Dimension object is placed inside the associated basic dimension or inspection box. |
PrefixString | Sets and returns the prefix string to be displayed along with the dimension text. |
PrimaryLowerTolerance | Sets and returns the text for the primary lower tolerance value. |
PrimaryToleranceSymbol | Sets and returns the text for the primary tolerance symbol of the referenced Dimension object. |
PrimaryUpperTolerance | Sets and returns the text for the primary upper tolerance value. |
ProjectionArc | Sets and returns the projection arc for the referenced Dimension object. |
ProjectionLineAngle1 | They return double values that represent the angle between the projection line and the x-axis of the sheet. |
ProjectionLineAngle2 | They return double values that represent the angle between the projection line and the x-axis of the sheet. |
ProjectionLineDirection | Specifies the projection line direction. |
RadialExtensionDistance | Sets and returns the extension distance of radial and half displayed diameter dimensions. Negative is away from the terminator. |
SecondaryLowerTolerance | Sets and returns the text for the secondary lower tolerance value. |
SecondaryUpperTolerance | Sets and returns the text for the secondary upper tolerance value. |
SecondValue | Returns the chamfer dimension angle. |
ShaftClassString | Shaft Class String. This string must match a class in the standards table, e.g. h7. |
StatusOfDimension | Returns the status(Detached, Error, Driving, Driven) of the referenced dimension object. |
Style | Sets and returns the active style on dimension |
Subfix2DisplayedText | Returns the evaluated Subfix2 text. |
SubfixAlignment | |
SubfixDisplayedText | Returns the evaluated Subfix text. |
SubfixString | Sets and returns the subfix text to be displayed along with the dimension text. |
SubfixString2 | Sets and returns the subfix2 text to be displayed along with the dimension text. |
SuffixDisplayedText | Returns the evaluated Suffix text. |
SuffixString | Sets and returns the suffix string to be displayed along with the dimension text. |
SuperfixDisplayedText | Returns the evaluated Superfix text. |
SuperfixString | Sets and returns the superfix text to be displayed along with the dimension text. |
SystemName | This read-only String property returns the system name for the referenced object. |
TerminatorPosition | Determines the position (inside or outside of the projection lines) of the terminator for the referenced Dimension object. |
TextScale | Sets and returns the text scale of the object. |
TrackAngle | Sets and returns the angle between the referenced Dimension object and the object it measures. |
TrackDistance | Sets and returns the track distance of the referenced Dimension object. |
True3DSketchDimension | Sets and returns the True3DSketchDimension property for the referenced dimension object. |
Type | Specifies the type of the object being referenced. |
UseStandardLimitAndFitTolerance | Extract tolerances from standards tables when TRUE. Use user-defined tolerances when FALSE. When TRUE, use appropriate DisplayType and use HoleClass and/or ShaftClass properties. |
Value | Sets or returns the value of the referenced Dimension object. |
VariableTableName | Returns the name used in the variable table. |
ZOrder | Specifies the front-to-back order in which an object is displayed relative to other objects. |