Solid Edge FrameworkSupport Type Library
OverrideChamferAngleString Property
Collapse All
Expand All
Solid Edge FrameworkSupport Type Library
>
Dimension Object
: OverrideChamferAngleString Property
Description
Returns the chamfer dimension angle override string.
Property type
Read-write property
Syntax
Visual Basic
Public Property OverrideChamferAngleString As String
Remarks
When the override string is set, the chamfer dimension displays this text string instead of the computed dimension value.
See Also
Dimension Object
|
Dimension Members