Solid Edge FrameworkSupport Type Library
ProjectionLineAngle2 Property
Collapse All
Expand All
Solid Edge FrameworkSupport Type Library
>
Dimension Object
: ProjectionLineAngle2 Property
Description
They return double values that represent the angle between the projection line and the x-axis of the sheet.
Property type
Read-only property
Syntax
Visual Basic
Public Property ProjectionLineAngle2 As Double
Remarks
For dimensions that do not have two projection lines, such as radial, coordinate, and chamfer dimensions, the values are identical.
See Also
Dimension Object
|
Dimension Members