Solid Edge Framework Type Library
Refraction Property
Collapse All
Expand All
Solid Edge Framework Type Library
>
FaceStyle Object
: Refraction Property
Description
Sets and returns the index of refraction for the referenced FaceStyle object. Only used in advanced render modes like raytracing.
Property type
Read-write property
Syntax
Visual Basic
Public Property Refraction As Single
Remarks
This property is used only in advanced render modes such as raytracing.
See Also
FaceStyle Object
|
FaceStyle Members