Solid Edge Framework Type Library
MatTable Object Members
Overview
Collapse All
Expand All
Solid Edge Framework Type Library
: MatTable Object
Public Methods
AddCustomProperty
AddMaterial
Adds material to material table.
AddMaterialToFavorites
AddMaterialToLibrary
ApplyMaterial
ApplyMaterialToDoc
ClearMRUList
CreateNewDirectory
CreateNewMaterialLibrary
DeleteCustomProperty
DeleteMaterial
DeleteMaterialFromLibrary
EditOpenGageExcelFile
This method is used to open the Gage file for editing.
ExportMaterialDataToFile
GetCountOfCustomProperties
GetCurrentGageName
This method is used to fetch the name of currently applied gage of a sheet metal document.
GetCurrentMaterialName
This method is used to fetch the name of currently applied material of a sheet metal document.
GetCustomMaterialPropertyFromDoc
GetCustomMaterialPropertyFromLibrary
GetDefaultGageFileName
This method is used to get the complete path of the gage excel file.
GetFavoriteMaterialList
GetMaterialLibraryFileList
GetMaterialList
GetMaterialListFromLibrary
GetMaterialPropValueFromDoc
GetMaterialPropValueFromLibrary
GetMaterialsFolderPath
GetMatLibFileName
GetMatPropValue
GetMRUMaterialLimit
GetMRUMaterialList
GetPSMGaugeInfoForDoc
This API is used to get all the gage related information from a sheet metal document.
GetPSMGaugeListFromExcel
This method is used to obtain list of Gages from a Gage table.
ImportMaterialDataFromFile
PerformGageDataValidation
This method is used to validate a Gage for data integrity.
RenameDirectory
RenameLibrary
RenameMaterial
SetActiveDocument
SetDocumentToGageTableAssociation
This method will create an association between the sheet metal file and the Gage table.
SetMaterialPropValueToLibrary
SetMaterialToGageTableAssociation
This method is used to create an association between a material and a Gage table.
SetMatPropValue
SetMRUMaterialLimit
UseNeutralFactorFromExcel
This method is used to decide source of the Neutral Factor.
WriteMaterialDataToXML
WriteMatLibFileFromXML
See Also
MatTable Object
|
Solid Edge V17 - What's New