Solid Edge Part Type Library : NormalToFaceCutout Object |
Delete | Deletes the referenced object. |
ExactRange | This method sets the exact range parameters for the referenced object. |
GetDimensions | Returns the Dimensions collection object for the referenced object. |
GetStatusEx | Returns the status of the specified object. |
GetStyle | Returns the feature style. |
Range | Returns the high and low range values for the referenced object. |
Reorder | Inserts the referenced object in front of or behind another feature. |
RollToFeature | Rolls the referenced Model object back to a specified feature. |
SetStyle | Sets the feature style. |
Application | Returns the active application object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
DisplayName | This read-only String property returns the display name for the referenced object. |
EdgebarName | This read-only property returns the Edgebar name of the referenced object. |
Edges | Returns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces. |
FaceContainment | Sets or gets the face containment property of the cutout |
Faces | Returns a collection of faces of a specified type that belong to a model, a feature, or a topology object. |
FacesByRay | Returns a collection of faces that are intersected by a specified vector. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
LongestCurveSide | Sets or gets the side of the longest curve, with reference to which to the cutout is placed |
ModelingModeType | Returns the modeling mode of the referenced object. |
Name | Returns the name of the referenced object. |
offsetDistance | Sets or gets the extent of the cutout |
Parent | Returns the parent object for the referenced object. |
ShowDimensions | Controls the display of dimensions for the feature object. |
Status | Returns the status of the specified object. |
Suppress | Temporarily suppresses the referenced object. |
SuppressVariable | Returns the suppress variable object. |
SystemName | This read-only String property returns the system name for the referenced object. |
Type | Specifies the type of the object being referenced. |