Solid Edge Part Type Library > Optimization Object : SetDesignConvergenceParameters Method |
Specify as a percent a relative amount that the design objective can deviate at convergence. The default value is 2.5. The valid range of values is 0 to 100.
The design is converged when the relative percentage change in the design objective value is less than the specified relative convergence value for two consecutive iterations. Also, when there is no design limit whose maximum violation has been exceeded in the last iteration
Visual Basic |
---|
Public Sub SetDesignConvergenceParameters( _ ByVal dMaxCnstrViolation As Double, _ ByVal dRelativeConvergence As Double, _ ByVal dAbsoluteConvergence As Double, _ ByVal dPerturbationFraction As Double _ ) |
Specify as a percent a relative amount that the design objective can deviate at convergence. The default value is 2.5. The valid range of values is 0 to 100.
The design is converged when the relative percentage change in the design objective value is less than the specified relative convergence value for two consecutive iterations. Also, when there is no design limit whose maximum violation has been exceeded in the last iteration