Solid Edge Part Type Library
SimplifiedAssemblyModel Object
Members 
Description
Simplified Assembly Model is the embedded document that contains all of the simplified assembly geometry for an assembly.
Object Model
SimplifiedAssemblyModel ObjectMeasureVariable ObjectApplication ObjectConstructions CollectionCoordinateSystems CollectionEdgebarFeatures CollectionDimensionStyles CollectionHoleDataCollection CollectionModels CollectionProfileSets CollectionRefAxes CollectionRefPlanes CollectionSketchs Collection
Example
Imports System.Runtime.InteropServices
Imports System.ComponentModel
Public Class SimplifiedAssemblyObject

    Private Sub Button1_Click(sender As Object, e As EventArgs) Handles Button1.Click

        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim objAssy As SolidEdgeAssembly.AssemblyDocument = Nothing
        Dim objSimpAssys As SolidEdgeAssembly.SimplifiedAssemblies = Nothing
        Dim objSimpAssy As SolidEdgeAssembly.SimplifiedAssembly = Nothing
        Dim objSimpModel As SolidEdgePart.SimplifiedAssemblyModel = Nothing
        Dim objEnclosures As SolidEdgePart.Enclosures = Nothing
        Dim objOccs As SolidEdgeAssembly.Occurrences = Nothing
        Dim objOcc As SolidEdgeAssembly.Occurrence = Nothing
        Dim objRef As SolidEdgeFramework.Reference = Nothing
        Dim objEnc As SolidEdgePart.Enclosure = Nothing
        Dim objSubOccs As SolidEdgeAssembly.SubOccurrences = Nothing
        Dim objSubOcc As SolidEdgeAssembly.SubOccurrence = Nothing
        Dim objModels As SolidEdgePart.Models = Nothing
        Dim objModel As SolidEdgePart.Model = Nothing
        Dim objConsts As SolidEdgePart.Constructions = Nothing
        Dim objMRefPlanes As SolidEdgePart.RefPlanes = Nothing
        Dim objMRefPlane As SolidEdgePart.RefPlane = Nothing
        Dim objType As Type = Nothing

        Dim occArray As System.Array = Array.CreateInstance(GetType(SolidEdgeFramework.Reference), 1)


        Try
            ' Create/get the application with specific settings
            objApplication = Marshal.GetActiveObject("SolidEdge.Application")

            If objApplication Is Nothing Then
                ' Get the type from the Solid Edge ProgID
                objType = Type.GetTypeFromProgID("SolidEdge.Application")
                ' Start Solid Edge
                objApplication = Activator.CreateInstance(objType)
                ' Make Solid Edge visible
                objApplication.Visible = True
            End If
            'Get reference to active document
            objAssy = objApplication.ActiveDocument()
            objOccs = objAssy.Occurrences
            objOcc = objOccs.Item(1)
            objSubOccs = objOcc.SubOccurrences
            For Each subocc As SolidEdgeAssembly.SubOccurrence In objSubOccs
                If (subocc.ThisAsOccurrence.Subassembly = False) Then
                    objSubOcc = subocc
                End If
            Next
            objRef = objSubOcc.Reference
            objRef = objAssy.CreateReference(objOcc, objSubOcc.ThisAsOccurrence)
            occArray(0) = objRef
            objSimpAssys = objAssy.SimplifiedAssemblies
            objSimpAssy = objSimpAssys.Item(1)
            objSimpModel = objSimpAssy.SimplifiedModel
            objMRefPlanes = objSimpModel.RefPlanes
            objMRefPlane = objMRefPlanes(1)
            objModels = objSimpModel.Models
            objModels.AddSimplifyEnclosure(1, occArray, objMRefPlane, SolidEdgePart.EnclosureTypeConstant.igEnclosureTypeBox, "body", objEnc)
            objModel = objModels(0)
            objEnclosures = objModel.Enclosures
            MsgBox(objEnclosures.Count)
        Catch ex As Exception
            MsgBox(ex.ToString)
        Finally

        End Try
    End Sub


End Class
See Also

SimplifiedAssemblyModel Members