Solid Edge Part Type Library > Thinwalls Collection : Add Method |
Visual Basic |
---|
Public Function Add( _ ByVal ThicknessSide As FeaturePropertyConstants, _ ByVal CommonThickness As Double, _ Optional ByVal OpenFaces As Variant, _ Optional ByVal NumberOfUniqueThicknesses As Variant, _ Optional ByVal UniqueThicknessesArray As Variant, _ Optional ByVal UniqueThicknessFaceListArray As Variant _ ) As Thinwall |
Value | Description |
---|---|
igAddRound | |
igAll | |
igAlongAnAxis | |
igAngularDummy | |
igAsConstruction | |
igBend | |
igBendAndFaceCornerRelief | |
igBendOnlyCornerRelief | |
igBoth | Feature Properties - Both |
igChainedCornerRelief | |
igChamfer2Setbacks | |
igChamfer45degSetback | |
igChamferAngleSetback | |
igCircular | |
igCloseCornerCircleCutout | |
igCloseCornerClosed | |
igCloseCornerNone | |
igCloseCornerOpen | |
igClosed | |
igCloseFaces | |
igConcave | |
igConstantRadiusArc | |
igConstRadiusRound | |
igContinuous | |
igConvex | |
igCopy | |
igCornerRound | |
igCounterboreHole | |
igCounterboreProfileIsAtBottom | |
igCounterboreProfileIsAtTop | |
igCounterdrillHole | |
igCountersinkHole | |
igCurvatureContinuous | |
igCurvatureContinuousInterior | |
igCurveSetSeperator | |
igDeleteFaceHeal | |
igDelSMFaceBoth | |
igDelSMFaceNone | |
igDelSystemRelief | |
igDelZeroBendRadius | |
igDevelopableSurface | |
igEdgeBasedCrossSection | |
igEdgesByLoop | |
igEdgesByVertex | |
igEnd | |
igEndCaps | |
igEqualOffset | |
igEquationType | |
igExtend | Feature Properties - Extend |
igExtendBendRelief | |
igFacesTouchingCurvesOnly | |
igFilletBendRelief | |
igFinite | |
igFlangeCenterOfEdge | |
igFlangeEndFromEndEdge | |
igFlangeEndOnEndEdge | |
igFlangeFromBothEndsOfEdge | |
igFlangeFromDefinedStartPoint | |
igFlangeFullEdge | |
igFlangeMatchFace | |
igFlangeOffset | |
igFlangeStartFromEndEdge | |
igFlangeStartOnEndEdge | |
igFlatten | |
igFormedEnd | |
igFromNonReferenceEnd | |
igFromReferenceEnd | |
igFromTo | |
igFull | |
igGroove | |
igHemTypeCenteredLoop | |
igHemTypeClosed | |
igHemTypeClosedLoop | |
igHemTypeCurl | |
igHemTypeOpen | |
igHemTypeOpenLoop | |
igHemTypeSFlange | |
igIgnoreBlends | |
igInside | Feature Properties - Remove/Add Material Inside |
igInsideDimension | |
igIntersect | |
igLancedEnd | |
igLeft | Feature Properties - Project to Left |
igLinear | |
igLinearCurvatureContinuousExtension | |
igLinearTangentExtension | |
igLip | |
igLouverFormedEndType | |
igLouverLancedEndType | |
igLouverRound | |
igLouverRoundNone | |
igMitreByAngle | |
igMitreByDist | |
igMitreManufacturingCut | |
igMitreNormalToThickness | |
igMitreParallelToThickness | |
igMitreRegularCut | |
igMove | |
igMultipleEdges | |
igNatural | |
igNeutralFactorFromExcel | |
igNFType | |
igNoCornerRound | |
igNoExtend | Feature Properties - Do Not Extend |
igNone | |
igNonSymmetric | |
igNormal | |
igNormalSideDummy | Feature Properties - Normal Side |
igNoRound | |
igNullConstant | |
igOffset | |
igOutside | Feature Properties - Remove/Add Material Outside |
igOutsideDimension | |
igOverlapFaces | |
igParallelDummy | |
igParallelToPlane | |
igPartingFromCurve | |
igPartingFromEdge | |
igPartingFromPlane | |
igPartingFromSurface | |
igPatternAlongCurve | |
igPatternCircular | |
igPatternFillRegion | |
igPatternMirror | |
igPatternMountingBoss | |
igPatternRectangular | |
igPatternUserDefined | |
igPeriodic | |
igProfileBasedCrossSection | |
igProjectOptionProject | |
igProjectOptionWrap | |
igPunchedEnd | |
igRadial | |
igRaisedCounterboreSlot | |
igRecessedCounterboreSlot | |
igRecreateBlends | |
igRectangularBendRelief | |
igReflective | |
igRegularHole | |
igRegularSlot | |
igRegularThread | |
igRemoveBoundaries | |
igRemoveExternalBoundaries | |
igRemoveInternalBoundaries | |
igReverseNormal | |
igReverseNormalSideDummy | Feature Properties - Reverse Normal Side |
igRight | Feature Properties - Project to Right |
igRipBendRelief | |
igRipCornerRelief | |
igRndCapAcrossSharpEdges | |
igRndMiterAtCorner | |
igRndPreserveTopologyOff | |
igRndPreserveTopologyOn | |
igRndRollAcrossSharpEdges | |
igRndRollAcrossTangentEdgesOff | |
igRndRollAcrossTangentEdgesOn | |
igRndRollAlongBlendEdgesOff | |
igRndRollAlongBlendEdgesOn | |
igRndRollAroundCorner | |
igRoundAllVertexSetback | |
igRoundEndVertexEdgeSetback | |
igRoundSetbackIsAbsolute | |
igRoundSetbackIsRelative | |
igRoundSingleVertexSetback | |
igRoundStartVertexEdgeSetback | |
igRoundVertexEdgeSetback | |
igShowBoundaries | |
igSideInfoSetSeperator | |
igSingleEdge | |
igSMClearanceCutout | |
igSMFaceCutout | |
igSMMidPlaneCutout | |
igSplit | |
igSplitAngle1Left | |
igSplitAngle1Right | |
igSplitDraft | |
igStart | |
igStepDraft | |
igStepDraftPerpendicular | |
igStraightPipeThread | |
igSubtract | |
igSweepAlignArcLength | |
igSweepAlignNormal | |
igSweepAlignParallel | |
igSweepAlignParametrically | |
igSweepC1Continuity | |
igSweepC2Continuity | |
igSweepMergeAll | |
igSweepMergeAlongPath | |
igSweepMergeNone | |
igSweepScaleNone | |
igSweepScaleStartAndEnd | |
igSweepTwistNone | |
igSweepTwistStartAndEnd | |
igSweepTwistTurns | |
igSweepTwistTurnsPerUnitLength | |
igSymmetric | Feature Properties - Symmetric Extent |
igTangent | |
igTangentInterior | |
igTaperByAngle | |
igTaperByRatio | |
igTaperByRLRatio | |
igTaperDimAtBottom | |
igTaperDimAtTop | |
igTaperedEnd | |
igTaperedHole | |
igTaperedPipeThread | |
igTaperedToPlane | |
igTappedHole | |
igThickness | |
igThkInProfilePlane | |
igThkNormalToProfilePlane | |
igThreeHundredAndSixty | |
igThroughAll | |
igThroughAxis | |
igToEndOfEdge | |
igToggleToConstruction | Toggle from Design to Construction |
igToggleToDesign | Toggle from Construction to Design |
igToKeyPoint | |
igToNext | |
igTreatmentCircleCutout | |
igTreatmentCrown | |
igTreatmentDraft | |
igTreatmentFormedFeatureDisplayAsCenterMark | |
igTreatmentFormedFeatureDisplayAsModeled | |
igTreatmentFormedFeatureDisplayAsSketch | |
igTreatmentFormedFeatureDisplayAsSketchAndCenterMark | |
igTreatmentIntersect | |
igTreatmentMiterRelief | |
igTreatmentOff | |
igTreatmentRectangularCutout | |
igTreatmentUCutout | |
igTreatmentVCutout | |
igUnequalOffset | |
igUnite | |
igUShaped | |
igVarRadiusRound | |
igVBottomDimToFlat | |
igVBottomDimToV | |
igVShaped | |
igWeldGrooveCapProject | |
igWeldGrooveCapSameAsTop | |
igWeldGrooveCapSurface |
Private Sub Form_Load() Dim objApp As SolidEdgeFramework.Application Dim objDoc As SolidEdgePart.PartDocument Dim objModel As SolidEdgePart.Model Dim objProfArr(1 To 2) As SolidEdgePart.Profile Dim objLines As SolidEdgeFrameworkSupport.Lines2d Dim objRelns1 As SolidEdgeFrameworkSupport.Relations2d Dim objThnWls As SolidEdgePart.Thinwalls Dim objFaces As Object Dim objFaceArr(1 To 3) As SolidEdgeGeometry.Face Dim dblThkArr(1 To 3) As Double Dim lngNum As Long Dim lngStatus As Long ' Report errors Const PI = 3.14159265358979 ' Create/get the application with specific settings On Error Resume Next Set objApp = GetObject(, "SolidEdge.Application") If Err Then Err.Clear Set objApp = CreateObject("SolidEdge.Application") Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument") objApp.Visible = True Else Set objDoc = objApp.ActiveDocument End If ' Draw the Profile Set objProfArr(1) = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(1)) Set objLines = objProfArr(1).Lines2d Call objLines.AddBy2Points(x1:=0, y1:=0, x2:=0.04, y2:=0) Call objLines.AddBy2Points(x1:=0.04, y1:=0, x2:=0.04, y2:=0.04) Call objLines.AddBy2Points(x1:=0.04, y1:=0.04, x2:=0, y2:=0.04) Call objLines.AddBy2Points(x1:=0, y1:=0.04, x2:=0, y2:=0) ' Relate the Lines to make the Profile closed Set objRelns1 = objProfArr(1).Relations2d Call objRelns1.AddKeypoint(Object1:=objLines(1), Index1:=igLineEnd, Object2:=objLines(2), Index2:=igLineStart) Call objRelns1.AddKeypoint(Object1:=objLines(2), Index1:=igLineEnd, Object2:=objLines(3), Index2:=igLineStart) Call objRelns1.AddKeypoint(Object1:=objLines(3), Index1:=igLineEnd, Object2:=objLines(4), Index2:=igLineStart) Call objRelns1.AddKeypoint(Object1:=objLines(4), Index1:=igLineEnd, Object2:=objLines(1), Index2:=igLineStart) ' Check for the Profile Validity lngStatus = objProfArr(1).End(ValidationCriteria:=igProfileClosed) If lngStatus <> 0 Then MsgBox ("Profile not closed") End If ' Create the Base Protrusion Object Set objModel = objDoc.Models.AddFiniteExtrudedProtrusion(NumberOfProfiles:=1, _ ProfileArray:=objProfArr, ProfilePlaneSide:=igRight, _ ExtrusionDistance:=0.04) objProfArr(1).Visible = False ' Check the status of Base Feature If objModel.ExtrudedProtrusions(1).Status <> igFeatureOK Then MsgBox ("Error in the Creation of Base Protrusion Feature object") End If ' Create a ThinWall object Set objThnWls = objModel.Thinwalls Call objThnWls.Add(ThicknessSide:=igOutside, CommonThickness:=0.01) ' Check the status of Thinwall Feature If objThnWls(1).Status <> igFeatureOK Then MsgBox ("Error in the Creation of ThinWall object with ThicknessSide = igOutside") End If ' USER DISPLAY ' Release objects Set objApp = Nothing Set objDoc = Nothing Set objProfArr(1) = Nothing Set objProfArr(2) = Nothing Set objModel = Nothing Set objLines = Nothing Set objRelns1 = Nothing Set objThnWls = Nothing Set objFaces = Nothing End Sub