Private Sub Form_Load()
Dim objApp As SolidEdgeFramework.Application
Dim objDoc As SolidEdgePart.PartDocument
Dim objModel As SolidEdgePart.Model
Dim objProfArr(1 To 2) As SolidEdgePart.Profile
Dim objLines As SolidEdgeFrameworkSupport.Lines2d
Dim objRelns1 As SolidEdgeFrameworkSupport.Relations2d
Dim objThnWl1 As SolidEdgePart.Thinwall
Dim bShowDimns As Boolean
Dim lngStatus As Long
' Report errors
Const PI = 3.14159265358979
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
' Draw the Profile
Set objProfArr(1) = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(1))
Set objLines = objProfArr(1).Lines2d
Call objLines.AddBy2Points(x1:=0, y1:=0, x2:=0.04, y2:=0)
Call objLines.AddBy2Points(x1:=0.04, y1:=0, x2:=0.04, y2:=0.04)
Call objLines.AddBy2Points(x1:=0.04, y1:=0.04, x2:=0, y2:=0.04)
Call objLines.AddBy2Points(x1:=0, y1:=0.04, x2:=0, y2:=0)
' Relate the Lines to make the Profile closed
Set objRelns1 = objProfArr(1).Relations2d
Call objRelns1.AddKeypoint(Object1:=objLines(1), Index1:=igLineEnd, Object2:=objLines(2), Index2:=igLineStart)
Call objRelns1.AddKeypoint(Object1:=objLines(2), Index1:=igLineEnd, Object2:=objLines(3), Index2:=igLineStart)
Call objRelns1.AddKeypoint(Object1:=objLines(3), Index1:=igLineEnd, Object2:=objLines(4), Index2:=igLineStart)
Call objRelns1.AddKeypoint(Object1:=objLines(4), Index1:=igLineEnd, Object2:=objLines(1), Index2:=igLineStart)
' Check for the Profile Validity
lngStatus = objProfArr(1).End(ValidationCriteria:=igProfileClosed)
If lngStatus <> 0 Then
MsgBox ("Profile not closed")
End If
' Create the Base Protrusion Object
Set objModel = objDoc.Models.AddFiniteExtrudedProtrusion(NumberOfProfiles:=1, _
ProfileArray:=objProfArr, ProfilePlaneSide:=igRight, _
ExtrusionDistance:=0.04)
objProfArr(1).Visible = False
' Check the status of Base Feature
If objModel.ExtrudedProtrusions(1).Status <> igFeatureOK Then
MsgBox ("Error in the Creation of Base Protrusion Feature object")
End If
' Create a ThinWall object
Set objThnWl1 = objModel.Thinwalls.Add(ThicknessSide:=igOutside, CommonThickness:=0.01)
' Check the status of Base Feature
If objThnWl1.Status <> igFeatureOK Then
MsgBox ("Error in the Creation of ThinWall object")
End If
' Get the ShowDimensions Property of ThinWall object
bShowDimns = objThnWl1.ShowDimensions
objThnWl1.ShowDimensions = Not bShowDimns
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objProfArr(1) = Nothing
Set objProfArr(2) = Nothing
Set objModel = Nothing
Set objLines = Nothing
Set objRelns1 = Nothing
Set objThnWl1 = Nothing
End Sub