#define APPR_already_processed (EMH_APPR_error_base + 112) |
Cannot execute update package that is already processed.
Definition at line 308 of file appr_errors.h.
#define APPR_array_length_mismatch (EMH_APPR_error_base + 5) |
The revision-rules, in-dates and out-dates arrays should be the same length.
Definition at line 39 of file appr_errors.h.
#define APPR_attribute_already_mapped (EMH_APPR_error_base + 55) |
Returned by the appearance mapping create Instance method if an attribute of new mapping is already mapped.
Definition at line 248 of file appr_errors.h.
#define APPR_attribute_array_length_mismatch (EMH_APPR_error_base + 52) |
The attr-names and attr-values arrays should be the same length.
Definition at line 228 of file appr_errors.h.
#define APPR_attribute_name_not_unique (EMH_APPR_error_base + 51) |
Appearance attribute names must be unique. An attempt has been made to create a new attribute with the same name as an existing attribute.
Definition at line 225 of file appr_errors.h.
#define APPR_background_updater_has_never_run (EMH_APPR_error_base + 180) |
Definition at line 370 of file appr_errors.h.
#define APPR_background_updater_has_not_run_recently (EMH_APPR_error_base + 181) |
Definition at line 371 of file appr_errors.h.
#define APPR_background_updater_too_many_failures (EMH_APPR_error_base + 182) |
Definition at line 372 of file appr_errors.h.
#define APPR_callback_failed (EMH_APPR_error_base + 32) |
An Appearance callback function failed.
Definition at line 158 of file appr_errors.h.
#define APPR_cannot_ask_is_matching_appearance (EMH_APPR_error_base + 110) |
Need to have parent appearance and appearance root set to invoke isMatchingAppearance.
Definition at line 299 of file appr_errors.h.
#define APPR_cannot_select_primary_yet (EMH_APPR_error_base + 114) |
Cannot select a primary object whilst another is in process
Definition at line 314 of file appr_errors.h.
#define APPR_cannot_set_prop_when_populated (EMH_APPR_error_base + 25) |
You may not set this property on an appearance root that is associated with any appearances.
Definition at line 128 of file appr_errors.h.
#define APPR_cant_mix_date_and_unit_eff (EMH_APPR_error_base + 21) |
Appearance does not support context rev rules configuring by a mixture of date and unit effectivity. Unit effectivity + release date is the only mixed configuration mode supported.
Definition at line 106 of file appr_errors.h.
#define APPR_cant_mix_date_eff_and_rel (EMH_APPR_error_base + 22) |
Appearance does not support context rev rules configuring by a mixture of date effectivity and release date. Unit effectivity + release date is the only mixed configuration mode supported.
Definition at line 113 of file appr_errors.h.
#define APPR_corrupt_root (EMH_APPR_error_base + 24) |
The appearance root is associated with corrupt appearances.
Definition at line 122 of file appr_errors.h.
#define APPR_date_must_be_after_final_in_date (EMH_APPR_error_base + 9) |
When adding a date, it must be chronologically later than the final in-date.
Definition at line 51 of file appr_errors.h.
#define APPR_date_must_be_after_final_out_date (EMH_APPR_error_base + 10) |
When adding a date, it must be chronologically later than the final out-date.
Definition at line 54 of file appr_errors.h.
#define APPR_duplicate_pools (EMH_APPR_error_base + 2) |
There should be precisely one instance of the class AppearanceRootPool.
Definition at line 30 of file appr_errors.h.
#define APPR_empty_secondary_queue (EMH_APPR_error_base + 104) |
Secondary queue should always have at least one element.
Definition at line 270 of file appr_errors.h.
#define APPR_empty_where_clause (EMH_APPR_error_base + 20) |
It makes no sense to extend a WHERE clause by adding something of the form "AND value IN empty-list".
Definition at line 99 of file appr_errors.h.
#define APPR_error_disabled (EMH_APPR_error_base + 18) |
Appearances disabled (by ACS, or by preference).
Definition at line 87 of file appr_errors.h.
#define APPR_final_out_date_must_be_null (EMH_APPR_error_base + 6) |
You may not set the final out-date if it is not currently a null-date.
Definition at line 42 of file appr_errors.h.
#define APPR_final_out_date_must_not_be_null (EMH_APPR_error_base + 7) |
You may not add an in-date if the current final out-date is a null-date.
Definition at line 45 of file appr_errors.h.
#define APPR_in_date_must_be_before_out_date (EMH_APPR_error_base + 12) |
When setting the in-date, it must be chronologically earlier than the out-date.
Definition at line 69 of file appr_errors.h.
#define APPR_in_unit_no_must_be_le_out_unit_no (EMH_APPR_error_base + 14) |
When setting the in-unit-no, it must be <= than the out-unit-no.
Definition at line 75 of file appr_errors.h.
#define APPR_inconsistent_roots (EMH_APPR_error_base + 103) |
When two appearances that are supposed to be the same aren't.
Definition at line 267 of file appr_errors.h.
#define APPR_internal_error (EMH_APPR_error_base + 27) |
Some internal error occurred.
Definition at line 137 of file appr_errors.h.
#define APPR_invalid_appr_validation_entity_tag (EMH_APPR_error_base + 106) |
Tag supplied is not that of an existing or valid appearance validation entity object.
Definition at line 278 of file appr_errors.h.
#define APPR_invalid_appr_validator_tag (EMH_APPR_error_base + 107) |
Tag supplied is not that of an existing or valid appearances validator object.
Definition at line 283 of file appr_errors.h.
#define APPR_invalid_attribute_index (EMH_APPR_error_base + 54) |
Returned by the appearance attribute query method if an attribute index is not valid.
Definition at line 243 of file appr_errors.h.
#define APPR_invalid_attribute_name (EMH_APPR_error_base + 53) |
Returned by the appearance attribute query method if an invalid attribute name is input.
Definition at line 238 of file appr_errors.h.
#define APPR_invalid_attribute_name (EMH_APPR_error_base + 53) |
Returned by the appearance attribute query method if an invalid attribute name is input.
Definition at line 238 of file appr_errors.h.
#define APPR_invalid_occurrence_change_tag (EMH_APPR_error_base + 113) |
Tag supplied is not that of an existing or valid occurrence change object.
Definition at line 311 of file appr_errors.h.
#define APPR_invalid_precise_entry_usage (EMH_APPR_error_base + 37) |
A valid Appearance context must, if using the Precise entry, place that entry ahead of all others and ungrouped.
Definition at line 190 of file appr_errors.h.
#define APPR_invalid_update_package_tag (EMH_APPR_error_base + 105) |
Tag supplied is not that of an existing or valid update package object.
Definition at line 273 of file appr_errors.h.
#define APPR_missing_end_item (EMH_APPR_error_base + 3) |
You must specify an End Item.
Definition at line 33 of file appr_errors.h.
#define APPR_missing_pool (EMH_APPR_error_base + 1) |
There should be an instance of the class AppearanceRootPool.
Definition at line 27 of file appr_errors.h.
#define APPR_needs_v7_eff_mode (EMH_APPR_error_base + 30) |
In order to use a revision rule which contains effectivity entries, you need to be in V7 effectivity mode.
Definition at line 149 of file appr_errors.h.
#define APPR_new_aps_not_consistent_with_validator (EMH_APPR_error_base + 108) |
New appearances are not consistent with those expected by the validator.
Definition at line 288 of file appr_errors.h.
#define APPR_no_defined_pre_release_statuses (EMH_APPR_error_base + 36) |
Specified rule is not supported for use with Pre-Release Appearances, since for such use it must contain only "Has Status (some pre-release status) By Release Date" entries, but the System Administrator has not defined any such statuses.
Definition at line 184 of file appr_errors.h.
#define APPR_no_entity_exists_with_parent_ap (EMH_APPR_error_base + 111) |
Validator needs at least one appearance validation entity for which the parent appearance is known.
Definition at line 305 of file appr_errors.h.
#define APPR_no_mapping_logic_defined (EMH_APPR_error_base + 50) |
Returned by the appearance attribute update user exit when no logic has been written yet.
Definition at line 219 of file appr_errors.h.
#define APPR_no_more_search_licenses (EMH_APPR_error_base + 33) |
No licenses available for searching or all licenses have been used up
Definition at line 161 of file appr_errors.h.
#define APPR_no_primary_in_process (EMH_APPR_error_base + 118) |
Definition at line 325 of file appr_errors.h.
#define APPR_no_primary_selected (EMH_APPR_error_base + 116) |
No primary has been selected yet
Definition at line 320 of file appr_errors.h.
#define APPR_non_status_rule_entry (EMH_APPR_error_base + 23) |
A valid Appearance context must contain only "Has Status" and "End Item" entries, optionally grouped together.
Definition at line 119 of file appr_errors.h.
#define APPR_not_supported (EMH_APPR_error_base + 4) |
Not supported yet.
Definition at line 36 of file appr_errors.h.
#define APPR_noteworthy_errors_occurred (EMH_APPR_error_base + 120) |
Processing the package generated some noteworthy errors.
Definition at line 331 of file appr_errors.h.
#define APPR_notified_sa (EMH_APPR_error_base + 121) |
The SA has been notified (by email) about the errors.
Definition at line 334 of file appr_errors.h.
#define APPR_null_context_info_not_allowed (EMH_APPR_error_base + 16) |
When creating a context, all inputs must be non-null.
Definition at line 81 of file appr_errors.h.
#define APPR_out_date_must_be_after_in_date (EMH_APPR_error_base + 13) |
When setting the out-date, it must be chronologically later than the in-date.
Definition at line 72 of file appr_errors.h.
#define APPR_out_unit_no_must_be_ge_in_unit_no (EMH_APPR_error_base + 15) |
When setting the out-unit-no, it must be >= than the in-unit-no.
Definition at line 78 of file appr_errors.h.
#define APPR_precise_no_component_item_rev (EMH_APPR_error_base + 38) |
A Precise Appearance must reference the correct component item revision.
Definition at line 195 of file appr_errors.h.
#define APPR_primary_already_locked (EMH_APPR_error_base + 115) |
Another process already has the primary locked
Definition at line 317 of file appr_errors.h.
#define APPR_primary_not_finished (EMH_APPR_error_base + 117) |
Cannot complete the primary as it has secondaries waiting to be processed.
Definition at line 323 of file appr_errors.h.
#define APPR_query_array_length_mismatch (EMH_APPR_error_base + 17) |
The query-entries and query-values arrays should be the same length.
Definition at line 84 of file appr_errors.h.
#define APPR_rev_rule_edits_not_allowed (EMH_APPR_error_base + 19) |
A rev rule referenced by an appearance set cannot have entries other than date and unit added to or removed from it.
Definition at line 93 of file appr_errors.h.
#define APPR_rev_rule_is_locked (EMH_APPR_error_base + 40) |
An AppearanceRoot cannot be created for a revision rule that is currently locked.
Definition at line 207 of file appr_errors.h.
#define APPR_rev_rule_is_nested (EMH_APPR_error_base + 39) |
Appearances cannot be generated for revision rules that use nested effectivity.
Definition at line 201 of file appr_errors.h.
#define APPR_revision_rule_absent (EMH_APPR_error_base + 8) |
The supplied revision rule is absent from the appearance's list of revision-rules.
Definition at line 48 of file appr_errors.h.
#define APPR_unable_to_bootstrap_when_populated (EMH_APPR_error_base + 26) |
Internal error: a bootstrap package cannot be processed for an appearance root that is associated with any appearances.
Definition at line 134 of file appr_errors.h.
#define APPR_unit_eff_needs_end_item_entry (EMH_APPR_error_base + 31) |
A valid Appearance context must contain only "Has Status" and "End Item" entries, optionally grouped together.
Definition at line 155 of file appr_errors.h.
#define APPR_unknown_task (EMH_APPR_error_base + 119) |
The updater doesn't recognise the supplied task.
Definition at line 328 of file appr_errors.h.
#define APPR_unsuitable_pre_release_rev_rule (EMH_APPR_error_base + 34) |
Specified rule is not supported for use with Pre-Release Appearances, since for such use it must contain only "Has Status (some pre-release status) By Release Date" entries, but it has some other type of entry.
Definition at line 168 of file appr_errors.h.
#define APPR_unsuitable_pre_release_rev_rule_entry (EMH_APPR_error_base + 35) |
Specified rule is not supported for use with Pre-Release Appearances, since for such use it must contain only "Has Status (some pre-release status) By Release Date" entries, but it contains an entry with some other (non-pre-release) status.
Definition at line 176 of file appr_errors.h.
#define APPR_unsuitable_rev_rule (EMH_APPR_error_base + 11) |
Specified rule is not supported for use as an Appearance context. Following errors explains why:
APPR_needs_v7_eff_mode
APPR_non_status_rule_entry
APPR_cant_mix_date_and_unit_eff
APPR_cant_mix_date_eff_and_rel
APPR_rev_rule_is_nested
Definition at line 66 of file appr_errors.h.
#define APPR_update_mgr_buffer_overflow (EMH_APPR_error_base + 154) |
Definition at line 351 of file appr_errors.h.
#define APPR_update_mgr_connection_broken (EMH_APPR_error_base + 156) |
Definition at line 357 of file appr_errors.h.
#define APPR_update_mgr_connection_failed (EMH_APPR_error_base + 160) |
Definition at line 361 of file appr_errors.h.
#define APPR_update_mgr_connection_rejected (EMH_APPR_error_base + 162) |
Definition at line 363 of file appr_errors.h.
#define APPR_update_mgr_external_app_failed (EMH_APPR_error_base + 163) |
Definition at line 364 of file appr_errors.h.
#define APPR_update_mgr_idle_but_processing (EMH_APPR_error_base + 201) |
Definition at line 380 of file appr_errors.h.
#define APPR_update_mgr_idle_but_queue_not_empty (EMH_APPR_error_base + 200) |
Definition at line 379 of file appr_errors.h.
#define APPR_update_mgr_invalid_host (EMH_APPR_error_base + 159) |
Definition at line 360 of file appr_errors.h.
#define APPR_update_mgr_marshalling_failed (EMH_APPR_error_base + 151) |
Definition at line 348 of file appr_errors.h.
#define APPR_update_mgr_message_truncated (EMH_APPR_error_base + 153) |
Definition at line 350 of file appr_errors.h.
#define APPR_update_mgr_no_admin_email (EMH_APPR_error_base + 167) |
Definition at line 368 of file appr_errors.h.
#define APPR_update_mgr_no_config_file (EMH_APPR_error_base + 165) |
Definition at line 366 of file appr_errors.h.
#define APPR_update_mgr_not_idle_but_nothing_to_do (EMH_APPR_error_base + 202) |
Definition at line 381 of file appr_errors.h.
#define APPR_update_mgr_query_failed (EMH_APPR_error_base + 155) |
Definition at line 356 of file appr_errors.h.
#define APPR_update_mgr_socket_error (EMH_APPR_error_base + 150) |
Definition at line 347 of file appr_errors.h.
#define APPR_update_mgr_syntax_error_in_config (EMH_APPR_error_base + 166) |
Definition at line 367 of file appr_errors.h.
#define APPR_update_mgr_timed_out (EMH_APPR_error_base + 161) |
Definition at line 362 of file appr_errors.h.
#define APPR_update_mgr_timedout_waiting_for_finish (EMH_APPR_error_base + 203) |
Definition at line 382 of file appr_errors.h.
#define APPR_update_mgr_unauthorized_user (EMH_APPR_error_base + 164) |
Definition at line 365 of file appr_errors.h.
#define APPR_update_mgr_unexpected_reply (EMH_APPR_error_base + 157) |
Definition at line 358 of file appr_errors.h.
#define APPR_update_mgr_winsock_failed (EMH_APPR_error_base + 158) |
Definition at line 359 of file appr_errors.h.
#define APPR_update_mgr_wrong_message (EMH_APPR_error_base + 152) |
Definition at line 349 of file appr_errors.h.
#define APPR_updater_rel_stat_cannot_be_nulltag (EMH_APPR_error_base + 101) |
Appearances updater needs a release status
Definition at line 258 of file appr_errors.h.
#define APPR_updater_rel_stat_not_on_item_rev (EMH_APPR_error_base + 102) |
Any item revision added to an appearances updater must have a release status the same as that of the updater.
Definition at line 264 of file appr_errors.h.
#define APPR_validation_entity_without_parent (EMH_APPR_error_base + 109) |
Validation entity needs either a parent appearance or a parent bom line.
Definition at line 293 of file appr_errors.h.
#define APPR_validation_failed (EMH_APPR_error_base + 300) |
Definition at line 384 of file appr_errors.h.
#define APPR_validity_outside_parent (EMH_APPR_error_base + 28) |
The appearance's validity range is outside that of its parent.
Definition at line 140 of file appr_errors.h.
#define APPR_validity_overlap (EMH_APPR_error_base + 29) |
The appearance's validity overlaps that of a matching appearance.
Definition at line 143 of file appr_errors.h.