#include <schmgt_bridge_itk.h>
Definition at line 133 of file schmgt_bridge_itk.h.
The Schedule
Definition at line 135 of file schmgt_bridge_itk.h.
The UID of the User being added
Definition at line 136 of file schmgt_bridge_itk.h.
The membership level in that schedule. Valid values are-{0-observer,1-participant,2-coordinator}
Definition at line 137 of file schmgt_bridge_itk.h.
char* AddMembers_d::cost |
The cost value (n.nnn (15.3 max)
Definition at line 138 of file schmgt_bridge_itk.h.
char* AddMembers_d::currency |
The ISO-4217 currency code.
Definition at line 139 of file schmgt_bridge_itk.h.