Solid Edge Revision Manager Object Library
GetCachePath Method
Specifies the number of files for which to obtain cache paths.
Specifies the URL locations on a SharePoint server of the files for which to obtain cache paths.
Specifies the number of files for which cache paths were obtained.
Specifies the local user's cache paths for the specified files.
Description
This method returns the cache paths for the specified files.
Syntax
Visual Basic
Public Function GetCachePath( _
   ByVal numberOfFilesToGetPathFor As Long, _
   ByVal ListOfFilePaths As Variant, _
   ByRef numberOfFilesReturned As Long, _
   ByRef ListOfFilesContainingCachePaths As Variant _
) As Long
Parameters
numberOfFilesToGetPathFor
Specifies the number of files for which to obtain cache paths.
ListOfFilePaths
Specifies the URL locations on a SharePoint server of the files for which to obtain cache paths.
numberOfFilesReturned
Specifies the number of files for which cache paths were obtained.
ListOfFilesContainingCachePaths
Specifies the local user's cache paths for the specified files.
Example
Imports RevisionManager
Imports System.Runtime.InteropServices

Module Example

    Sub Main()
        Dim objApplication As RevisionManager.Application = Nothing
        Dim objInsight As RevisionManager.Insight = Nothing
        Dim aListOfFilePaths(1) As Object
        Dim NumberOfFilesReturned As Long
        Dim aListOfFilesContainingCachePaths As Object = Nothing

        Try
            ' Start Revision Manager.
            objApplication = New RevisionManager.Application

            ' Get reference to Insight object.
            objInsight = objApplication.Insight

            aListOfFilePaths(0) = "http://solidvm/Engineering/PreReleased/PreReleasedDocLib/Summit.par"
            aListOfFilePaths(1) = "http://solidvm/Engineering/PreReleased/PreReleasedDocLib/CDPlayer/CDPlayer.asm"

            objInsight.GetCachePath(aListOfFilePaths.Length, aListOfFilePaths, NumberOfFilesReturned, aListOfFilesContainingCachePaths)
        Catch ex As Exception
            ' Write any errors to console.
            Console.WriteLine(ex.Message)
        Finally
            ' Release COM Objects.
            If Not (objInsight Is Nothing) Then
                Marshal.ReleaseComObject(objInsight)
                objInsight = Nothing
            End If

            If Not (objApplication Is Nothing) Then
                objApplication.Quit()
                Marshal.ReleaseComObject(objApplication)
                objApplication = Nothing
            End If
        End Try
    End Sub

End Module
See Also

Insight Object  | Insight Members

Send comments on this topic.