| Item |
Description |
| PR 2208599 |
Can't use the StudyOwner.Count property in ST4 |
| PR 1914096 |
GetReferenceToGraphicMember2 returns a runtime error |
| PR 1915928 |
When opening an alternate assembly with the API function an exception occurs |
| PR 1888771 |
Resolved issues with Ribbon Bar Customizing |
| PR 1911009 |
Split Button & Drop Button doesn't work for macros |
| PR 2205600 |
Changing Drawing View Style by API is strange when the views are made in V20 |
| PR 2207742 |
NormalToFaceCutOuts.Add method does not return the expected result |